Tool/software: IMDS Node ID 1096264700 / 2.00 is rejected in IMDS system.
The IMDS record has been rejected. Please review and modify record as described below and re-submit data for acceptance.
1. In Component: IC AMP RtR SING LOW OFFSET SOT23…
Part Number: TDA4AEN-Q1 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hello TI,
SDK mcu_plus_sdk_j722s_10_01_00_22
I did below changes for can test on TDA4AEN board.
# \mcu_plus_sdk_j722s_10_01_00_22\examples\drivers\mcan\mcan_loopback_interrupt…
Part Number: TPS4810-Q1 Tool/software:
Customer would like to check whether TPS4810-Q1 can be used for 5 mosfets in parallel application.
The mosfet spec was below. Could you please help confirm?
Part Number: TCAN1044A-Q1 We are using the TCAN1044AVDRQ1 CAN transceiver in our design. The transceiver is powered with VCC = 5 V, and our MCU operates at 3.3 V logic.
Do we need any level shifting between the MCU (TXD/RXD) and the transceiver…
Part Number: TPS3890-Q1 Tool/software: Hello, Based on datasheet “5 Device Comparison Table”, my customer calculated VHYST [%]. (Please refer to the attached Excel file.) For most devices, calculated VHYST [%] is almost equal to VHYST(typ)= 0.575%. However…
Part Number: TPSM33620-Q1
Tool/software:
Hi,
from the evm layout example, Figure 4-5 , it seems that these pins are not connected together with a trace. I just want to confirm if this is the case
this is what i have right now:
btw, what…
Part Number: TCAN1044A-Q1 Tool/software: Dear team,
Can we apply VIO which is used for TCAN1044AVDRQ1 to 5pin of TCAN1044ADRQ1? D/S mentions it is NC(=Not internally connected; Devices without VIO).
The background of this query is because my customer…
Part Number: ADC09QJ1300-Q1 Tool/software: Table 6-16, 6-17 and 6-18 in the data sheet does not show the max for the input clock range for JMODE 5. The non-Q100 version of the data sheet shows this max at 1040 MHz. I'm supporting an application which…
Part Number: DRV8163-Q1 Hi team,
What is device configuration difference between figure 6-4 and 6-5 or 6-6 and 6-7? We are using DRV8163H-Q1.
Figure 6-4 says it does not need RESET pulse to enter STANDBY mode on wakeup event. On the other hand, Figure…