There are RS-232 transceivers that need external high-voltage supplies, e.g., SN75155.
But in practice, high-noise environments are much easier handled with differential signals like LVDS (e.g., SN65LVDS049) or RS-422/RS-485 (e.g., SN65C1168E or 2× THVD1512…
Part Number: SN65LVDS049 http://www.ti.com/lit/mo/sllc163/sllc163.ibs
I'm trying to use the IBIS model above in Hyperlynx SI VX.2.3_Update2 . I've copied the data from the link into an .ibs file but when I go to assign the model, I get several errors…
Part Number: SN65LVDS049 Other Parts Discussed in Thread: ISOW7842 Icc of SN65LVDS049 datasheet is wrote a Typ:17mA/Max35mA. Is this Icc a device total current of SN65LVDS049?
Our customer are considering use SN65LVDS049 with Isolated supply voltage of…
Part Number: SN65LVDS049 Other Parts Discussed in Thread: DS90LV049 hello
I need to select a Dual-LVDS Differential Drivers and Receivers,SN65LVDS049 and DS90LV049 are almost same,
In my case,all LVDS lanes will be transfered on 100R twisted pair cable(4…
Part Number: SN65LVDS049 Hello,
There isn't a junction limit listed on the data sheet for the following part: SN65LVDS049PW.
Would I just take the storage temperature of 150 deg C, as explained in this link? [FAQ] What is the maximum junction temperature…
Part Number: SN65LVDS049 When I look at Table 2 "Receiver Truth table", I get confused.
In column one it says "Rin- - Rin+"
I interpret the other pictures in the datasheet, for example Figure 6 and Figure 11 in such a way that Rout…
Part Number: SN65LVDS049 Hi,
We are using SN65LVDS049 in our application. But we are confused with the pull down value of Enable bar (pin 9) pin. Can anyone help me with this.
Part Number: SN65LVDS049 Other Parts Discussed in Thread: DS90LV049 Hi all Would you mind if we ask SN65LVDS049? Do you have any experience to use SN65LVDS049 with Flat cable? Off course, we think it depends on cable length and attenuation. Kind regards, Hirotaka…
The SN65C1167 supports up to 18.5 MHz, depending on the load. Please show an oscilloscope trace of the A/B signals.
There are faster RS-422 transceivers like the THVD1552/THVD1452, for up to 25 MHz. If that is not enough, use LVDS, e.g., SN65LVDS049/DS90LV049…
Part Number: SN65LVDS049SN65LVDS049 schematic.pdf Some percent of the SN65LVDS049 show this error:
Hello all,
We have a problem with an LVDS Driver and Receiver SN65LVDS049, where I would like to ask for your help. We are currently at the production…