Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SN65LVDS116 Other Parts Discussed in Thread: SN65LVDS105 , I have a design where I plan on generating a reference clock using a 64MHz CMOS oscillator, which I then bring to a SN65LVDS105 (CMOS to 4x LVDS). Three of the SN65LVDS105's outputs…
Part Number: SN65LVDS105 Hello Team, can you provide phase noise for this part, please? Signalfrequency = 40MHz.
Are the typ. 23mA (RL=100Ohm) the current for the whole device?
Thanks and Best Regards, Hans
Part Number: SN65LVDS105 Other Parts Discussed in Thread: DSLVDS1048 To whom it may concern,
I am using the SN65LVDS105D to convert TTL clock to LVDS. Is there any suggested part as LVDS receiver to pair with SN65LVDS105D. Therefore, I can convert the LVDS…
Part Number: SN65LVDS105 Hi,
I have a question with regards to SN65LVDS105.
In our circuit, there is a 25Mhz clock at the input pin but if we want to totally disable all the output. To minimise any EMI radiation and unwanted current flow, how should we…
Thanks Amy, this has been very helpfull. I will be making a testprint with both the SN65LVDS105 and the DS90LV047A to see which component works best under my expected conditions.
Have a good weekend!
Part Number: SN65LVDS105 Dear,
I want to use 2 SN65LVDS105 LVDS Repeaters to have 8 similar outputs to serve for a fixed 50 MHz LVDS compatible clock signal.
My clock signal is generated by a MiniZed board. The output of the MiniZed is 3.3 V.
My question…
Other Parts Discussed in Thread: SN65LVDS105 , DS90LV011A , DS90LV017A Hello
I would like to have Solution for converting Signal format from TTL(3.3V) to LVDS(1.8V).
SN65LVDS105 can convert TTL(3.3V) to LVDS(3.3V) only but its function is not included f…
Other Parts Discussed in Thread: SN65LVDS105 Hi,
Below value is measured with Vid=±100mV, but the input of SN65LVDS105 is LVTTL level, it should be in Via, not Vid.
My input is Via magnitude is over 3V as below shows.
The differential output…
Hello, all:
Sorry but I need some additional data on maximum recommended junction temperatures for SN65LVDS105PWR.
The data sheet lists recommended ambient temperature of -40 to +85C, but not recommended maximum junction temperature. Customer is calculating…