Part Number: SN65LVDS31-EP Hello,
For the SN65LVDS31MDREP I had two questions:
Based on other TI data sheets, is it safe to assume theta-JC in this data sheet means top-case?
Is there unpublished theta-JB? Or just theta-JA and theta-JC?
Part Number: SN65LVDS31-EP Hello E2E Experts,
Good day.
I found SN65LVDS31-EP which covers the temperature range (-55'C to 125'C) and works with 3.3V nominal.
Do you see any reason for the incompatibility between this and my original AM26LV31ID…
Part Number: SN65LVDS31 Dear Sir/Madam,
I want to design a SPI to LVDS connection over 2.5 meters using SN65LVDS31 (Transmit) and SNL65LVDT33 (Receive with internal terminating resistor).
i'm considering fews methods of doing the 2.5 meters inter connection…
Part Number: SN65LVDS31 Hi
I would like to request for the Junction-to-Case (Top) thermal resistance (Theta_JC (Top)) information for SN65LVDS33PWR
Thank you!
Part Number: SN65LVDS31-33EVM Other Parts Discussed in Thread: SN65LVDS31 , Hello I would like to find out if there is something similar to this evaluation board SN65LVDS31-33EVM that would be 5V tolerant on the inputs of the driver chip. Ideally I am looking…
Part Number: SN65LVDS31 Hi, I would like to check for SN65LVDS31PWR:
1. If the maximum absolute and/or operating junction temperature is available?
2. If the values for Junction-to-case (top) thermal resistance (R_thetaJC(top)) and Junction-to-ambient…
Part Number: SN65LVDS31 Other Parts Discussed in Thread: SN65LVDS33 Hi,
Please help to check schematic using SN65LVDS31 & SN65LVDS33PW.(as below pic)
Thank you.
Part Number: SN65LVDS31-EP Other Parts Discussed in Thread: SN65LVDS31
Hi Team,
Good day. Our customer is using the SN65LVDS31MDREP to translate a 3.3V Clock signal to LVDS.
For this project, they need to compute the jitter added by each device. The jitter…
Part Number: SN65LVDS31
Dear team,
The signaling rate discribed in the SN65LVDS31 datasheet is 400Mbps.
However, the minimum signaling rate discribed in the Application Note (SLLD009) is 600Mbps.
Which is the better way of thinking?
Yours Sincerely…
Part Number: SN65LVDS31 I need a SPICE model of SN65LVDS31, but only the IBIS Model is available on the official website. Can someone provide me one? Thanks.