Part Number: SN65LVDS31-EP Is it necessary to have an output series resistor on the LVDS outputs when driving a 100ohm differential load?
Output load is shown to be 5 ohms so a 45-ohm series resistor should help with reflections?
- Michael
Part Number: SN65LVDS31-EP Hello,
For the SN65LVDS31MDREP I had two questions:
Based on other TI data sheets, is it safe to assume theta-JC in this data sheet means top-case?
Is there unpublished theta-JB? Or just theta-JA and theta-JC?
Part Number: SN65LVDS31-EP Hello E2E Experts,
Good day.
I found SN65LVDS31-EP which covers the temperature range (-55'C to 125'C) and works with 3.3V nominal.
Do you see any reason for the incompatibility between this and my original AM26LV31ID…
Part Number: SN65LVDS31-EP Other Parts Discussed in Thread: SN65LVDS31
Hi Team,
Good day. Our customer is using the SN65LVDS31MDREP to translate a 3.3V Clock signal to LVDS.
For this project, they need to compute the jitter added by each device. The jitter…
Part Number: SN65LVDS31-EP Hi Support,
The data sheet did not include HBM/CDM.
Please tell me the test results of ESD.
-Part#:
SN65LVDS31MDREP
SN65LVDS33MDREP
-HBM: ? V
-CDM: ? V
Best Regards;
Hideyuki
Part Number: SN65LVDS31-EP Hi Team, In one of our customer's application they need to provide information concerning the fault tolerance of SN65LVDS31-EP. In cases of failure of the LVDS receiver (end-device), 3.6V will be directly applied to the differential…
Part Number: SN65LVDS31-EP Other Parts Discussed in Thread: SN65LVDS31 , SN65LVDS33-EP , Hello,
I am using a SN65LVDS31 on my design and I would like to know what is the maximum voltage tolerate by the differential output without degradation ? The synoptic…
Part Number: SN65LVDS31-EP Other Parts Discussed in Thread: SN65LVDS31 Hi team,
Good day. Our customer is requesting for the ESD HBM rating for V62/07627-01XE. Is the ESD HBM rating of non-EP version which is SN65LVDS31 applicable?
Regards, Carlo
Part Number: SN65LVDS31-EP Other Parts Discussed in Thread: SN65LVDS33-EP Hello,
Can you tell me if the SN65LVDS31-EP and SN65LVDS33-EP are BiCMOS or CMOS device?
I am considering using them in a CubeSat and radiation effects depends on the technology…
Part Number: SN65LVDS31-EP Hi team,
My customer wants to know differential output tr/tf minimum and maximum values. But these values are not described in the datasheet.
If you have the data, Please let me know the values.
・Data Sheet: www.ti.com/.../sn65lvds31…