Part Number: SN65LVDS33 Other Parts Discussed in Thread: SN65LVDS31 , , SN65LVDS31-32BEVM Good afternoon,
I have sn65lvds31 on one of my board(I dont have this board yet) and sn65lvds33 on one of my other board. I would like to test sn65lvds33 by creating…
Part Number: SN65LVDS31-EP Hi Support,
The data sheet did not include HBM/CDM.
Please tell me the test results of ESD.
-Part#:
SN65LVDS31MDREP
SN65LVDS33MDREP
-HBM: ? V
-CDM: ? V
Best Regards;
Hideyuki
Part Number: SN65LVDS33 Hi
What will happen in case one of the LVDS input line is now disconnected (or the POS [A] or the NEG [B] ) and left floating
while the opposite pin keeps working as usual?
Will the receiver still present the proper value (maybe…
Part Number: SN65LVDS33-EP Hi team,
My customer is looking for 6bit LVDS receiver which supports ~105degC. They can accept 4bit+2bit or 8bit devices as well.
Their requirement is 60MHz and Vcc=3.3V. I believe that SN65LVDS33-EP x2pcs would meet their…
Part Number: SN65LVDS33 Other Parts Discussed in Thread: SN65LVDS31 , Hello expert, My customer plan to use SN65LVDS33 and SN65LVDS31 for SPI over LVDS application for below spec's SPI. ・SPI Freq: 15MHz ・Direction: Bi-directional ・ FFC length: 1~2m Then, I…
Part Number: SN65LVDS33 Other Parts Discussed in Thread: TIDA-060017 , , ADS8910B Hi team,
My customer would like to build a SPI buffer solution with our SN65LVDS33 which has mentioned in TIDA-060017.
And, there is also a application note which is talking…
Part Number: SN65LVDS33 Other Parts Discussed in Thread: SN65LVDS049 , AM26C32 Hi Team, Good day. Our customer is looking for the theta_JC of the following part numbers:
SN65LVDS33PWRG4 SN65LVDS049PW AM26C32IPW We would really appreciate if you could help us…
Part Number: SN55LVDS33-SP Other Parts Discussed in Thread: SN65LVDS33 , , SN65LVDS31 , SN55LVDS31-SP Does the the SN55LVDS33-SP use the same basic die (albeit with different processing, packaging, testing and specifications) compared to the SN65LVDS33? …
Part Number: SN65LVDS33-EP Original details: 2 questions on the SN65LVDS33-EP (i.e. SN65LVDS33MDREP), Quad LVDS Diff Line Rx 1. I am using this part to convert a differential LVDS 100 MHz clock to TTL for a frequency measurement on a scope. Can you tell…