Part Number: SN65LVPE502 Other Parts Discussed in Thread: TUSB522P Hi sir,
My customer is using SN65LVPE502 USB3 and adjust EQ to 15dB, but cause LFPS Vtx-DIFF-PP too low (spec. 08.v~1.2v).
Is there any way to solve this issue?
Thank you.
Part Number: SN65LVPE502 Other Parts Discussed in Thread: TUSB522P Hi,
I had implemented SN65LVPE502 on my project. When I plugged in USB3.1 GEN2 device, the system only found USB2.0 device,
but I plugged in USB3.1 GEN1 device, the system could find USB3…
Part Number: SN65LVPE502 Hello,
We applied USB compliance test which SN65LVPE502 is on the board and the result is failed as below items.
TD.1.1 No LFPS output
TD.1.2 No LFPS output, there is a waveform like CP0
TD.1.3 passed
TD.1.4 passed
TD.1.5 No loopback…
Part Number: SN65LVPE502 Other Parts Discussed in Thread: TUSB522P About USB3.0 Compliance test for SN65LVPE502, please let me know about two points below condition;
①Should SN65LVPE502 set to Compliance mode for pass the USB3.0 compliance test?
(Can…
Other Parts Discussed in Thread: SN65LVPE512 , SN65LVPE502 My customer T is interested in an USB3.0 redriver and have a little question about the TI redrivers:
Are the SN65LVPE512 and the SN65LVPE502 based on the same silicon, because the datasheets are…
Other Parts Discussed in Thread: SN65LVPE502CP , SN65LVPE502 , SN65LVPE502A , SN65LVPE512 Dear Specialists
My customer is thinking SN65LVPE502CP.
He wants to know the difference between SN65LVPE502 and SN65LVPE502CP.
According to the datasheets, the differences…
Sure but, how do i proceed to attach schematic files to my answer and make sure these remain pretty confidential (even if there is no secret in the schematic around SN65LVPE502...)?
Other Parts Discussed in Thread: SN65LVPE502 Hello Experts,
I am curious if i can use the SN65LVPE502 to redrive a USB2.0 signal. I am looking at using the USB2.0 Phy on the OMAPL137 and I would like to run it to the other side of the board and through…
Other Parts Discussed in Thread: SN65LVPE502 , SN65LVPE502A Hello,
I'd like to know whether it's possible to use two sn65lvpe502 devices to build an active USB 3.0 cable. The idea is to re-drive the signals from both host and device side. The signal quality…