Part Number: SN65LVPE512 Other Parts Discussed in Thread: TUSB522P
Hi,
I have integrated 2 SN65LVPE512 TI USB 3.0 re-drivers in my design as depicted in the picture below.
In order to optimize the configuration of the EQ, OS and DE I inject from BERT…
Part Number: TUSB522P Other Parts Discussed in Thread: SN65LVPE512 ,
Hi,
We change TI USB 3.0 re-driver solution from SN65LVPE512 to TUSB522P, however, pin6&18 is connected to GND without any layout modification.
It works fine with our function test…
Part Number: SN65LVPE512 Other Parts Discussed in Thread: SN65LVPE502A Dear Specialists,
My customer is considering SN65LVPE512, but it's NRND now
He'd like to know why.
Could you please break it down for him?
I appreciate your great help in advance…
Part Number: SN65LVPE512 Other Parts Discussed in Thread: TUSB501 Team-
We have an application where only one side of the SN65LVPE512 is needed, RX1 => TX1.
What is the appropriate way to terminate RX2N:P and TX2N:P so that the device doesn't shut…
Part Number: SN65LVPE512 Other Parts Discussed in Thread: TUSB522P Dear Specialists,
My customer is considering SN65LVPE512 and has an inquiry.
Could you please advise?
---inquiry
The datasheet describes typical application, the device is set host s…
Other Parts Discussed in Thread: SN65LVPE512 , TUSB522P , TUSB1002 Hi @ all,
in a current design we use the SN65LVPE512 for the host and the device side.
Now we have problems with the negotiation of the USB 3.1 device and if the negotiation is successful…
Other Parts Discussed in Thread: SN65LVPE512 , TUSB522P USB3.0 cable with two SN65LVPE512
Hello,
I'd like to know whether it's possible to use two SN65LVPE512 devices to build an active USB3.0 cable. The idea is to re-drive the signals from both…
Other Parts Discussed in Thread: SN65LVPE512 , TUSB522P HI Team,
Do we have SN65LVPE512 simulation Model 64 bit version?
I find below but it is 32 bit only. Customer needs 64 bit
http://www.ti.com/lit/zip/sllc441
Thanks
Sam
Hello,
I have a basic question.
It is mentioned Pin labeled 'Controller' must connect to the host or controller on the Datasheet.
I checked the Block diagram of the device. It looks the 'Controller' side function is same as 'Connector' side function…
Other Parts Discussed in Thread: SN65LVPE512 , SN65LVPE502 My customer T is interested in an USB3.0 redriver and have a little question about the TI redrivers:
Are the SN65LVPE512 and the SN65LVPE502 based on the same silicon, because the datasheets are…