Then the ACT240 is a good solution. If the input signals are not TTL, you can use the SN74AC240 instead. For a non-inverting buffer, use the SN74AC244/SN74ACT244.
Part Number: SN74LVC244A Other Parts Discussed in Thread: SN74AC244 , SN74LVC2G125 Hello Team,
while supply and input voltage are specified exactly with the same values in the abs max ratings I wonder why the supply is specified with 3.6V and Vin with 5…
Are you suggesting to use a SN74AC244 part? So ganging all inputs therefore outputs together should be fine and give enough current. I am placing a 39ohms series driving the cable, therefore max sink/source would be around 125mA. What is the gates output…
Part Number: SN74ACT244 Other Parts Discussed in Thread: SN74AC244 Hi expert,
The normal operation voltage for SN74ACT244 is 4.5V~5.5V. Could you tell what the state of the output stage will be if the VCC is 3V~4.5V?