Part Number: SN74AHC14 HI Sir
If I want to use SN74AHC14 to design smith trigger
Could I use below same equation to calculator R320 and C458's value ?
Thanks
Part Number: SN74AHC14 Other Parts Discussed in Thread: SN54AHC14 Hi,
SN74AHC14 Data-Sheet(SCLS238L) page7 there is an empty space only in the tPHL portion of "6.7 Switching Characteristics-5V". (tPHL: From A (input) to Y (output), CL=15pF: column…
Part Number: SN74LVC04A Other Parts Discussed in Thread: SN74LVC14A , SN74AHC14 Hi Team,
The customer needs to get the max VOH value and the min VOH value for SN74LVC04A SN74AHC14 and SN74LVC14A.
The customer's requirements are when VCC is 3.3V and IOH…
Part Number: SN74HC14 Other Parts Discussed in Thread: SN74AHC14 , SN74LVC14A , SN74HCS04 Hi Experts,
Good day! I need your assistance regarding the customer's inquiry below. Here are the full details below.
I am using the SN74HC14D. The supply voltage…
Yes, CD4000 devices have clamping diodes from the inputs to V CC . The absolute maximum ratings forbid voltages above V CC + 0.5 V; a diode current larger than 10 mA can damage the device.
The AHC and LV-A families run at 5 V and have overvoltage-tolerant…
Part Number: SN74AHCT14 Other Parts Discussed in Thread: SN74AHC14 , SN54AHCT14 , SN54AHCT14-SP , , Dear Team,
The Cpd of SN74AHCT14 is 112pF (typ).
However, the Cpd of a close series, SN74AHC14, is 9pF (typ).
I don't know the temperature conditions for…
Other Parts Discussed in Thread: SN74AHC14 We are doing some failure analysis and testing of diodes external to this part and want to make sure we do not damage this part.
If we have a 26 mA current source at the '1A' input pin of the SN74AHC14 will…
The LVC devices have -Q1 variants.
The SN74AUP1G07 could be replaced with the SN74AUC1G07 or SN74LVC1G07 (with different supply voltage ranges).
The SN74AHC14 could be replaced with the SN74LV14A.
Other Parts Discussed in Thread: SN74AHC14 Hello,
I was testing a old control board and observed that, SN74AHC14 is seeing an input of +/- 7.5V. -7.5V is being clamped to -0.7. And 7.5V input is read as is. SN74AHC14 is supplied from 3.3V supply rail. …