Part Number: SN74AHC244-Q1
Tool/software:
These parts share a similar datasheet but I wanted to verify if the dies are identical despite the package differences.
Part Number: SN74AHC244-Q1
Hi,
Looking at the datasheet, there are differences in TAPE DIMENSIONS with and without G4. Is this correct?
I saw the post below and thought there was no difference between G4 and no G4.
So please also tell me why…
Hello Ishiwata-san,
I checked through the SN74AHC244QPWRQ1 versus the SN74AHC244QPWR and found that these two are the same device - physical construction, electrical characterization, and qualifications are all identical.
The only difference I can…
The TXS OE inputs are active high, so I would have expected pull-down resistors. Do you intend these devices to be active during power-up/-down (when the I/O states might be undefined)?
The TXS has internal pull-up resistors at the I/Os. The external…
Part Number: SN74AHC244 Hello Team,
I'm checking the TSSOP package for the SN74AHC244 .
All the ordering parts are up to 85C while in the datasheet is written that the recommended operative temperature is up to 125C.
Can you clarify the mismatch…
Part Number: SN74HCS7002-Q1 Other Parts Discussed in Thread: SN74HCS02-Q1 , SN74AHC244 , SN74CBT1G384 , SN74CBT1G125 , SN74AHC541 Hi Team,
My customer is looking at our HCS logic family, checking the datasheet SN74HCS7002-Q1 and SN74HCS02-Q1 have the…
Part Number: SN74AHC244 The datasheet for the subject AHC device states that undershoot (input voltages that go below 0 V) must be constrained to -.5V (must be no more negative than -.5V) OR of the undershoot goes more negative than -.5V, then the input…