Part Number: SN74AHCT1G125-Q1 Hello team,
Please help explain the difference between 74AHCT1G125DBVRE4 and SN74AHCT1G12DBVR? I can not got it from datasheet.
Best regards,
Lanxi Li
Part Number: SN74AHCT1G125 Hello,
We use SN74AHCT1G125 on several of our boards. We are seeing a short between pins 3 and 4. Have you seen this before? What could cause this?
Eric K.
Part Number: SN74AHCT1G125-Q1 Hi,
Could you help to check if this part meets AEC-Q standard? (the ordering part number is: CAHCT1G125QDCKRQ1)
The datasheet says it is "Qualified for Automotive Applications", but I can't find any keyword about…
Part Number: SN74AHCT1G125 Hi team,
In the customer’s system, 5.25V at output pin might be inputted. Customer understand the situation is over absolute max range but they would like to understand the failure mode if the situation happed.
Could…
Part Number: SN74AHCT1G125 Hi,
I think that ψjt of DCK package is so low compared to other devices.
How condition was this measured?
Best Regards,
Kuramochi
Part Number: SN74AHCT1G125-Q1 Hi,
I plan to design with SN74AHCT1G125-Q1 in a Vcc = 3.3V application.
However, i can only find the VIH/VIL spec under Vcc = 3V and 4.5V - 5.5V condition in the datasheet.
Could you let me know how to estimate the VIH/VIL…
Part Number: SN74AHCT1G125 Hi,
My customer is considering using SN74AHCT1G125.
Why is the capacitance different between a single supply and multiple supplies as below?
Best Regards,
Kuramochi
Part Number: SN74AHCT1G125 Hi,
My customer is considering using SN74AHCT1G125.
ΔIcc is specified as below;
Does it mean that Icc is maximum when input voltage is around 3.4V?
Best Regards,
Kuramochi
Part Number: SN74AHCT1G125 Other Parts Discussed in Thread: SN74LVC1G17 Hi,
Is there any possibility that penetration current is flown when the input pin is opened?
Best Regards,
Kuramochi