Part Number: SN74LVC541A Other Parts Discussed in Thread: SN74AHCT541 Is 5V ok to be applied to pin 20 Vcc of SN74LVC541APWR? The recommended is 3.3V, but I see the max rating is 6.5V. So does that mean 5V Vcc is ok? That means the output will be 5V with…
To convert 5 V to 3.3 V, you can use any buffer with overvoltage-tolerant inputs, such as the SN74AHC367. To convert 3.3 V to 5 V, you can use any buffer with TTL-compatible inputs, such as the SN74AHCT367.
(8-bit devices like the SN74AHC541/SN74AHCT541…
TTL-compatible CMOS inputs are designed to have practically no shoot-through current for 3.3 V signals:
For 7 channels, I'd suggest the SN74AHCT244 or SN74AHCT541.
Part Number: SN74F541 Other Parts Discussed in Thread: SN74AHCT541 Hello Guys,
Good day.
Need your help to confirm logic compatibility between these two parts:
XC7A200T-2FBG676C-LVCMOS (Driver) (VOH&VOL: 2.9 & 0.4) and SN74F541DW-LVCMOS (Receiver) (VIH&VIL…
Yes, a load that is too large looks like this.
If the signals are unidirectional, a direction-controlled translator like the SN74LVC8T245 will work much better. (AXC does not go above 3.3 V.) But for 3.3 V → 5 V translation, you could simply use a buffer…
Part Number: TXS0108E Other Parts Discussed in Thread: SN74LVC8T245 , SN74LVC2T45 , SN74AHCT125 , SN74AHCT1G125 , SN74AHCT541 , SN74LVC2G34
Hi,
my customer need level shift for SPI and UART. And they may need 1 SPI master(3.3V) and several SPI slaves(5V)…
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LVC8T245 , SN74AHCT541 Hi team,
My customer looks for LVTTL to TTL level shifter (greater than 4bit is preferable).
For now, I'm promoting SN74LVCC3245A.
Could you please propose any successor…
That 50 mA value is the allowed current flowing through the closed switch, which happens only for the input at GND, and relies on the drive strength of the external device.
A current of 0.33 mA through the 10 kΩ pull-up resistor would result in a voltage…
Part Number: TXB0108 Other Parts Discussed in Thread: SN74AHCT541
Hi,
can I use TXB0108 as unidirectional level translator from 3.3V to 5V
Warm regards,
Monisha om