Part Number: SN74ALVC164245 Tool/software: Hello,
I am considering to use SN74ALVC164245DGGR as a level shifter. We have a question about the max output current that is listed in the datasheet. Is the output current listed as a total for the entire…
Part Number: SN74ALVC164245 Other Parts Discussed in Thread: TXB0108 Hi,
Could you please let me know minimum input drive current (Iih) for 16 BIT level translator part# SN74ALVC164245 . Not able to find the value in datasheet.
FYI: For TI 8-bit Level…
Part Number: SN74ALVC164245 Hi,
For our customer design, we need the land pattern (or footprint) of the product part number SN74ALVC164245DGG. Can you share the relevant document? Unfortunately, the information contained in the datasheet is not enough…
Part Number: SN74ALVC164245 Hi,
Customer would like to adopt SN74ALVC164245 for JTAG of RTG4.
its max frequency is 25MHz.
Does SN74ALVC164245 support this frequency?
Thanks.
Part Number: SN74ALVC164245 Hello,
My Team considers to use the IC with VCCA=3.3V, VCCB=5V.
He made prototype board and one concern is that he pulled up DIR pin to VCCB whereas datasheet states DIR pin reference to VCCA.
Is there any problem for…
Part Number: SN74ALVC164245 For the mentioned part, I would like to know 3 things, 1. Total mass in grams 2. Combustible mass in grams 3. Whether the products are UL 94 V0 certified or not
Part Number: SN74ALVC164245 Hi,
can you help me with checking the SN74ALVC164245ZRDR? I have some de-soldered samples that has very low operating temperature. Temperature over 50°C shout down outputs on 2B1 and 2B2 from ~5 V to 0,2 V. It start working…
Part Number: SN74ALVC164245 Hi,
In one of our legacy design, we found Direction Pin 1 and Pin 25 of level Translator (SN74ALVC164245DLR) is connected to +5V and board is working. Whereas datasheet says "If DIR high is needed (A data to B bus), ramp…