Part Number: SN74AUC1G125 Tool/software: Hi expert,
The datasheet for SN74AUC1G125YZPR specifies the Voh minimum at 1.65V and 8mA drive current as 1.2V
Do you have data for the Voh minimum across process and temperature operating at 1.8V and ~200uA…
Part Number: SN74AUC1G125 Other Parts Discussed in Thread: SN74AUC2G125 , SN74AUC125 , SN74AUC244 , SN74AUP1G125 , SN74AUP2G125 Tool/software:
I find out SN74AUC1G125, a tri-state buffer with output enable that works fine at VCC=1.0V. However, the Vih…
Part Number: SN74AUC1G125 Hi,
On data sheet, 10ns/V is max. SR at 1.8V. So the rising / rising time will be 10*1.8 = 18ns, right? In other words, the max. freq. is 1/36ns = 27.78MHz only at 1.8V. Is it correct?
Is there part suggestion for 125MHz…
Part Number: SN74AUC1G125 Hello Technocrats ,
The following buffer is used from PHY to iDRAC.
Currently, TI-SN74AUC1G125DCKR is being used as the main source without any issues.
I would like to inquire if TI-SN74AUP1G125DCKR is also suitable for…
Part Number: SN74AUC1G125 Dear Team,
how critical is this requirement to have the buffer in high impedance during powering up?
May a non-high impedance state of the buffer during powering-up harm the IC somehow?
Thank you,
Michael
Part Number: SN74AUC1G125 Hello expert,
Customer would like to use SN74AUC1G125 in eSPI application and want to know if SN74AUC1G125 can do bidirectional operation. May we have your help to answer that question? Thanks a lot!
Best regards,
Ann …
Part Number: SN74AUC2G125 Other Parts Discussed in Thread: SN74AUC1G125 , Hi Team,
My customer would like to check the bus frequency the SN74AUC2G125/SN74AUC1G125 can support. Will these devices support 50M?
Best regards
Ella
Part Number: SN74AUC1G125 Hello team,
Customer found Auc1g125inc.inc is messy code, so whether we have updated version about it? and do we have use guide about the connection?
Thanks.
Antony
Part Number: SN74AUC1G125 Other Parts Discussed in Thread: SN74LVC1G125 For both of these devices: SN74AUC1G125、 SN74LVC1G125 Can xOE have an input signal (High) before Vcc gets powered?
Taken from the DS:
To ensure the high-impedance state during…