Part Number: SN74AUP1G08 Hi team, I can not find package information for SN74AUP1G08DRYR (SON (DRY) | 6). Could you tell me about "PACKAGE OUTLINE","EXAMPLE BOARD LAYOUT","EXAMPLE STENCIL DESIGN" ? Sincerely. Kengo.
Part Number: SN74AUP1G08
Dear experts,
Our partner is trying to approve the SN74AUP1G08DCKR for a new project at approval stage
They brought small qty from Arrow and Digikey. They observed that the 2 parts have different die although they were with the…
Part Number: SN74AUP1G08
We recent bought SN74AUP1G08DCKR from distributors and realized differences in DIE code.
Can i check if both die codes are valid? is there any PCN on these differences?
Both are COO China and DC21+
DIE CODE = HEC - is this valid…
Part Number: SN74AUP1G08 Hi Team,
a customer is looking for an AND gate like SN74AUP1G08 but with even lower Icc rating.
Could you recommend a solution?
BR, Stefan
Part Number: SN74AUP1G08-Q1 Dear team,
My customer uses A pin to connect 1.8V signal, and B pin to connect 3.3V signal while their VCC is 1.8V. Is it ok?
Our input support 3.6V, so it should be ok in my understanding. But I am not sure whether it has bad…
Part Number: SN74AUP1G08 Hello I am considering using the SN74AUP1G08DBVR as a 3.3V to 1.8V translator on a power good signal. I will power the part with 1.8V and have a 3.3V and a 1.8V input and want to get a 1.8V output. Will this work?
Part Number: SN74AUP1T08 Other Parts Discussed in Thread: SN74AUP1G08 , Hi, Good day. Our customer is using the SN74AUP1T08 in their design however they are having supply issue and hey want to know if they can use the SN74AUP1G08 instead. Would that be fine…
Part Number: SN74AUP1G08 Hi,
is it possbile/acceptable to drive temporarily external voltage (3.3V) on output (Y) while SN74AUP1G08 itseld is driving LOW? 3.3V is applied to VCC while inputs A and B are LOW.
It seems to be working in logic wise that…
Part Number: SN74AUP1G08-Q1 Dear Logic team,
My customer is working on BMS for E-scooter. In the design, they used our SN74AUP1G08QDCKRQ1 which the lead time of the device is too long (>35 weeks). The customer is rush in their MP schedule, can you help…
Part Number: SN74AUP1G08-Q1 Hi, Team,
Customer want to know the output status for SN74AUP1G08-Q1 in following scenarios.
1. The VCC power down 3.3v -> 0V, one of the input has 3.3V voltage, how about the output status? Is there any sink current at the…