Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74GTLPH1655 Team,
I want to check if SN74AVC16T245 can support hot-swap. If it can't, any other level shifter can support? Thanks!
BR,
Qiang
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: TVP5158 , , TXV0108 , TXV0106 Tool/software: I am using the SN74AVC16T245 to translate +3.3V output of the TI TVP5158 Video Decoder to +1.8V to match an FPGA I/O. The 10 bit data is being clocked…
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: TXV0108 Tool/software: Hi,
We need the Voltage Translator for the RGMII, the voltage from 3.3V to 1.8V, and we need the speed to 1000Mbps MAX and 8# or 16# bit channels,
please kindly promote…
Part Number: SN74AVC16T245 TI Team,
How much channel to channel variation (delay) is expected on these parts? We are looking for expected variances to help with PCB trace matching decisions.
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: TXV0108-Q1 , TXV0106-Q1 Is there data for the channel to channel propagation delay skew for the SN74AVC16T245?
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74LVC3G07 , SN74LVC2T45 , SN74LXC1T14 We are plannig to use this buffer SN74AVC16T245 to control the different LEDs.
8 bicolor LEDs will sink 20mA current each from buffer SN74AVC16T245.…
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74AXC8T245 Hi,
This is Venkat from IIT-Madras, India.
We sourced about 25 SN74AVC16T245 ICs for our design over the last one month through Mouser.
We checked a few parts and found that…
Part Number: SN74AVC16T245 Hi Logic Team,
Can you please provide the following information for the TVSOP SN74AVC16T245? I do not see it in the datasheet.
Total power dissipation spec
Best regards, Nic Gough
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74AUC244 Hello
SN74AVC16T245 an support 80MHz clock signal. From B -> To A
VCCA=1.8V
VCCB=2.5V
Thanks
Roi