Part Number: SN74AVC4T774 Other Parts Discussed in Thread: SN74AXC4T774 Hello,
We are developing an USB 2.0 camera based on the Onsemi AR0144CS image sensor connected to a Cypress FX2 USB controller CY7C68013A. Image sensor works at 2.8V and USB controller…
Part Number: SN74AVC4T774 Other Parts Discussed in Thread: SN74AXC4T774 , TXS0104E Hi Expert,
I would like to confirm with you that customer used SN74AVC4T774RSVR and TXS0104EPWR for SPI/SMI level shift in the new design board.
And want to check if these…
Part Number: SN74AVC4T774 Hi Team,
Several questions regarding schematic design :
1. VCCA and VCCB doesn't require which side voltage level must be higher or equal to the other side, right ? 2. If DIR needs to be PU, it must be pull to VCCA side by…
Part Number: SN74AVC4T774 Other Parts Discussed in Thread: TMUX1111 Hi Team,
Can you please help us with this concern of our customer.
Regarding the differences in Recommended layout diagram for the following parts :
The parts are available in 16 PIN…
Part Number: SN74AVC4T774
Could you tell me the operating frequency (max) for the following voltages ?
1.VCCA : +1.2 [V] / VCCB : +1.2 [V]
A port -> B port
B port -> A port
Part Number: SN74AVC4T774 Hii TI Team I am working with SN74AVC4T774 buffer. I wanted to know whether the IC will get damaged if we don't provide supply on both the power rails but we have 3.3V on the output bus pins.
Part Number: SN74AVC4T774 Other Parts Discussed in Thread: SN74AVC4T245 , , TXU0304 , TXU0104 , TXU0204 Hello TI support team,
I would like to use sn74avc4t774 to replace sn74avc4t245 in a TDM/I2S application. I need to use the sn74avc4t774 also for the MCLK…
Part Number: SN74AVC4T774 Hi team,
Just wanted to make sure, when OE is high, all outputs are placed in the high-impedance state and the VCC isolation feature ensures that if either VCC input is at GND, then both ports are in the high-impedance state…
Part Number: SN74AVC4T774 hi Sir
May i know the diff between SN74AVC4T774RGYR & SN74AVC4T774RSVR?
only package different?
or material different ?
thanks
Part Number: SN74AVC4T774 Hi team,
I'm Ives Li, FAE in SZ AA1 team.
My customer TCL is using SN74AVC4T774 in their application as showed below:
And they found that the MISO input from SPI1 cannot be pulled down by SoC and SPI2, it will affect the…