Part Number: SN74AVCH4T245-EP Hello,
We bought the following component : CAVCH4T245MRSVREP. And I'm looking for the qualification report with some traceability informations. The batch we bought is on DC 2202 and lot code 27P5RNJ, 21P63KJ.
Underneath…
Part Number: SN74AVCH4T245-Q1 Tool/software: Team,
My customer is asking whether SN74AVCH4T245-Q1 have AEC-Q100 certification. Because it is not claimed in datasheet.
If no, please recommend similar part which pass AEC-Q100. Thanks.
Part Number: SN74AVCH4T245-Q1 Hi Team,
Please help to provide the below details regarding 74AVCH4T245QPWRQ1:
What is the Maximum Junction Temperature (Tj) for this part?
Does these components use less than 50nm feature technology? If yes, the…
Part Number: SN74AVCH4T245-Q1 Other Parts Discussed in Thread: SN74AVCH4T245 Tool/software: Hi,
In order to do some signal integrity simulations, I am looking for the IBIS model of the following component reference : SN74AVCH4T245-Q1
Could you please…
Part Number: SN74AVCH4T245 Other Parts Discussed in Thread: SN74AVC4T245 , SN74AXC4T245 , TXU0304 Hi Team,
We are using the SN74AVCH4T245 Level translator part in our schematics. We are using the same part in four instances. I had attached all the schematic…
Part Number: SN74AVCH4T245 Other Parts Discussed in Thread: SN74LVC1G125 Hi,
The customer encountered the following problems in use, please help to solve them.
1. The following SPI interface, one master and two slave, SN74AVCH4T245RSVR output impedance…
Part Number: SN74AVCH4T245 Hello team,
What will happen to this device if the Vcc became lower than minimum recommended operating condition of 1.2V - 3.6V.
Best Regards, Kei Kuwahara
Part Number: SN74AVCH4T245 You show stock on part # 74AVCH4T245RSVR -NT. Can you tell me what the NT at the end means? I need urgently P/N 74AVCH4T245RSVR. Please advise.
Ref 101-16927
Thanks.
Doris
Part Number: SN74AVCH4T245
Hi team,
As shown in the picture below, the customer has an I2S signal and wants to pass through the buffer.
Can they use the SN74AVCH?Connect both VCCA / VCCB in the picture below to 3.3V ?
Part Number: SN74AVCH4T245-EP Hi team,
Helping someone on this device. I need to know the max value for prop delay as he is trying to translate between 1.2V and 1.8V.. Is there any data to show the max for this spec? We are using the -EP device.
…