Part Number: SN74AVCH4T245 Other Parts Discussed in Thread: SN74LVC1G125 Hi,
The customer encountered the following problems in use, please help to solve them.
1. The following SPI interface, one master and two slave, SN74AVCH4T245RSVR output impedance…
Part Number: SN74AVCH4T245 Hello team,
What will happen to this device if the Vcc became lower than minimum recommended operating condition of 1.2V - 3.6V.
Best Regards, Kei Kuwahara
Hi Michael,
Thanks for your valuable feedback.
As per your suggestion we had updated the schematics and changed the part From SN74AVCH4T245 to SN74AVC4T245. Please find the Images attached below for the updated schematics.
Thanks and Regards
- Teja
…
Part Number: SN74AVCH4T245-EP Hi team,
Helping someone on this device. I need to know the max value for prop delay as he is trying to translate between 1.2V and 1.8V.. Is there any data to show the max for this spec? We are using the -EP device.
Thanks…
Part Number: SN74AVCH4T245-EP Hi Team,
The datasheet of CAVCH4T245MRSVREP states that “Active bus-hold circuitry holds unused or undriven inputs at a valid logic state. Use of pullup or pulldown resistors with the bus-hold circuitry is not recommended…
Part Number: SN74AVCH4T245 Other Parts Discussed in Thread: SN74AXCH4T245 Guys, does TI have the min and max data of tPLH, tPHL base on SN74AVCH4T245 1.2 to 3.3V? D atasheet just show the typ. data as below picture.
Thanks in advance!
Part Number: SN74AVCH4T245 Other Parts Discussed in Thread: SN74AXC4T245-Q1 , SN74AXCH4T245 Dear Team,
We are using 74AVCH4T245BQ-Q100 in our design and we need FFF alternate for this chip.
Can you please suggest best alternative in terms of direct replacement…
Part Number: SN74AVCH4T245 You show stock on part # 74AVCH4T245RSVR -NT. Can you tell me what the NT at the end means? I need urgently P/N 74AVCH4T245RSVR. Please advise.
Ref 101-16927
Thanks.
Doris
Part Number: SN74AVCH4T245-EP Hello
What is the output impedance of B-port outputs, if the A-port is driven at 3.3V and the B-port at 2.5V?
Best Regards
Tino
Part Number: SN74AVCH4T245
Hi team,
As shown in the picture below, the customer has an I2S signal and wants to pass through the buffer.
Can they use the SN74AVCH?Connect both VCCA / VCCB in the picture below to 3.3V ?