Other Parts Discussed in Thread: TIDA-010019 , SN74CBTLV16292 , TMUX1108 , TMUX1136 , TMUX1308 Hi team,
My customer is looking for MUX for multi-channel temperature sensor, and I’d like to ask your advice.
The system (for 1CH) would be like the one…
No.
When you exceed the absolute maximum ratings, the device might get damaged. When you exceed the recommended operating conditions, the device might not work.
You must use a device rated for 2.5 V. The largest are SN74CBTLV16292 with 12 channels, or…
Part Number: AM5726 Other Parts Discussed in Thread: SN74CBTLV16292 , CDCLVC1102 We are creating a design based on AM335X_ICE Eval Board (Made by TI), the big differences is Processor and interfaces. In this design PRU MII and MII interfaces are used,…
Part Number: SN74CBT16214 Other Parts Discussed in Thread: SN74CBTLV16292 , Are SN74CBT16214 and SN74CBTLV16292 able to pass 120MHz bit-rate bus signals (not the max switching rate allowed on logical control pins) ? Where can I check the bandwidth of these…
Part Number: SN74CBT16211C Other Parts Discussed in Thread: SN74CBTLV16292 Hi team,
Could you please recommend a suitable 1:2 bus switch for TFT-LCD module (R0-R7, G0-G7 and B0-B7 data signals, 24 bits)? Thanks!
Best regards,
Sam Ting
Part Number: SN74CBT16233 Other Parts Discussed in Thread: SN74CBTLV16292 , TS5MP645 Hi, Team,
SN74CBT16223 datasheet explains below specification. The min voltage of VIH is 2V. Does it for A-signal, B-signal, SEL and TEST?
Regards, Nagata.
Hi Rahul,
I would hesitate to use SN74CB3T16212 to pass 1.8V logic because the input and output of this device is not linear. It has build-in level shifting feature. It will be very convenient for rail-to-rail input/output. However, in your case, you…
Our largest mux is 1 to 16 so we cant help much there.
Here are some options for the 1 to 2.
SN74CBT162292 , SN74CBTLV16292 , SN74CBT16292 12 bit 1to2
SN74CBT16233 16 bit 1to2
Other Parts Discussed in Thread: TXB0108 , SN74AVCA164245 , SN74CBTLV16292 Dear Tier,
I have one question about SN74AVCA164245 and TXB0108.
One of my customer is using SN74AVCA164245 for SRAM interface. But as you know, SN74AVCA164245 needs direction control…