Part Number: SN74GTL1655 Hi team,
My customer met an output ringing issue when using SN74GTL1655. Below is the test data.
When input (BLue) is slowly ramping in the slew rate of ~2.3V/ms, the output (green) will generate a pulse rather than a simple step…
Part Number: SN74GTL1655 Hi team,
I read datasheet of SN74GTL1655, and found A port & B port can both be active when OEAB/ & OEBA/ are both low.
Does it mean that it supports auto-direction translation between two sides?
Thank you!
Part Number: SN74GTL1655 Hello Team,
My customer used our SN74GTL1655, signals transfer from B side to A side, below our the signal of B side, there is big glitch, it is OK? Pin64 (CLK) is pulled up to 3.3V, how does our part sample? edge or level? T…
Part Number: SN74GTL1655 Hello Team,
My customer uses our SN74GTL1655DGGR, the schematic is as below. They use two signals, and find the signals don't transfer from A side to B side. They test 2A3 and 2A8, both are 3.3V high level, but both 2B3 and 2B8…
Part Number: SN74GTL1655 Hi team,
My customer find when they power up the SN74GTL1655, there is a spur occur when the supply voltage go to about 70% VCC.(see below)
The blue on is the supply voltage, the yellow one is the output signal in 1A.(below is…
Part Number: SN74GTL1655 Hi team,
My customer use the part in the switch. And below is the diagram.
The signal is from the A port to B port.
And they find the B port signal has a ringing in the falling edge.(show as below).
So please help to answer…
Part Number: SN74GTL1655 Hi team,
My customer find that after powering on the chip, the output of A port will generate a serial of random signal when the B port is logic high.
The schematic is as below:
And the output signal is the purple one.
Could you…
Part Number: SN74GTL1655 Hi Team,
What's the input and output signal status when the VREF of SN74GTL1655DGGR was decrease to ground? Will the device output any error signal?What's the high and low voltage judgement level if the VREF is zero?…
Hi Shreyas,
Do you mean below description on SN74GTL1655's datasheet? Yes, customer would like this feature.
Do we have other choice? supporting over 25Mhz and 16bit is preferred.
Thanks.