Part Number: TXS0108E Other Parts Discussed in Thread: LSF0108 , TXB0108 , SN74GTL2003 Hi Team,
My customer is looking for 8 bit directionless voltage level translator, the required speed is 50M. I searched at TI.com, it comes out with TXS0108, LSF0108…
Part Number: SN74GTL2003 Other Parts Discussed in Thread: TXB0108 , TXS0108E , SN74LVC2T45 , SN74AVC2T45 , LSF0108 How do you calculate the pull up resistors for the SREF port when the input voltage can vary from 1.2V to 3.3V, form an FPGA module source. And…
Part Number: SN74GTL2003 I need to connect four SPI devices (two of them are 5V logic and another two are 3.3v logic) to 5v logic microcontroller.
i am thinking about use GTL2003, but I am not sure if it will work correct.
I am not sure about MISO line…
Hi,
I am interested in the timing mismatch from one channel to the next. My application is a unidirectional voltage translation from 3V3 to 1V8, with 3V3 on Dn side and 1V8 on Sn side.
I have 4 critical signals that need to match very well. A fixed…
Hi,
I couldn't find any information about bidirectional HSTL to LVTTL interfacing with that device? Has anybody experience this in designs?
Thanks.
Abacuss..
Other Parts Discussed in Thread: SN74GTL2003 Since I need to connect SD card to 5V microcontroller, I want to know if this can be accomplished using SN74GTL2003 8-bit auto direction sense voltage translators, and are threre any desing considerations when…