Part Number: SN74HC165-Q1 Dear TI Technical Support Team,
We are currently preparing for a surge test on a circuit designed with the SN74HC165-Q1. I am contacting you because I have an inquiry regarding the specifications in the device's datasheet.…
Part Number: SN74HC165-Q1 Hi, Team.
My customer, YURA is currently preparing for surge testing of a circuit under development that uses the SN74HC165-Q1.
In this regard, customer has a question regarding the device specifications in the datasheet…
Part Number: SN74HC165-Q1 Other Parts Discussed in Thread: SN74HCS165-Q1 Hi, Team
I've recommended SN74HC165-Q1 as the replacement of Nexperia, "74HC165D-Q100".
But, Customer is worrying about ESD rate of SN74HC165-Q1, 1500V vesus Neperia, 2000V.…
Part Number: SN74HC165-Q1 Hi team,
We are working on a replacement for NEX. During testing, the customer found that for SN74HC165QPWRG4Q1, when the system enters sleep mode (without supplying power to the chip), there is still about 0.9V at the VCC…
Part Number: SN74HC165-Q1 Tool/software: HI,
We received different lead frame on DC2343 and DC2503,
DC2343 samples bought from TI direct,
DC5503 bought from Arrow
there is no PCN to talk about lead frame on DC2343 and DC2503,
is this deemed…
Part Number: SN74HC165-Q1 Tool/software: Hi
Can you tell me the main difference between SN74HC165QPWR G4 Q1 and SN74HC165QPWRQ1 ?
I can't find in datasheet.
Thanks.
Luke
Part Number: SN74HC165-Q1 Tool/software: Hi Team
We bought from distributor recently and noticed a difference in the lead frames based on the 2 date codes we received.
Can we confirm if such difference in lead frame is deemed normal and does not affect…
Part Number: SN74HC165-Q1 Hi,
Our customer plans to use the SN74HC165QPWRG4Q1 at VCC = 3.3V.
However, this data sheet ( www.tij.co.jp/.../sn74hc165-q1.pdf) only lists AC characteristics, DC characteristics, and timing charts at VCC = 2V, 4.5V, and…
Part Number: SN74HC165-Q1 Hi Team
We designed SN74HC165-Q1 for fan motor monitoring.
When the switch is turned off, the B-EMF of the motor flows into the logic input pin of the SN74HC165-Q1.
A reverse voltage of about 43V(max) flows for 10us.…
Part Number: SN74HC165-Q1
HI team.
My customer designed SN74HC165-Q1 without connecting GND.
They proceeded to mass production with a mistaken circuit.
But, It does operate actually output depending on Input.
So, customer has question how did…