Part Number: SN74HC573A-Q1 Hi Experts,.
SN74HC573A-Q1 is used in customer for BMS. The project is under DV. There is fault output of SN74HC573A-Q1, it will cause the whole system down.
This device need be fixed before 9/10. So it can catch the PV test…
Part Number: SN74HC573A Hi,
We encounter intermittent uncertain wave from latched output pins.
Normal output is 5v level and keep expect latched time,but appear short pulse under 2~3v while defect occurs.
The compares waveform as attached.
Moreover,due…
Part Number: SN74HC573A
Hi all Would you mind if we ask SN74HC573A? <Question1> How much is absolute maximum and minimum input voltage (XD, LE and /OE)? -0.3V to Vcc? <Question2> Do input pins have any protection diodes between Vcc and input and…
Part Number: SN74HC573A-Q1 Hi Expert,
The engineer is asking the SN74HC573A-Q1 spec of High-level input voltage when VCC=3.3V.
Pls advice.TKS.
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan Limited
O: +886-2-2175-2582
…
Part Number: SN74HC573A Our customer just received a new batch of SN74HC573ADWR parts. The data sheet on page 14 shows NiPDAu (Nickel-Palladium-Gold) as leads finish. Usually the visual look of the leads looks like silver chrome. The leads of the new parts…
Part Number: SN74HC573A-Q1 Hi, team,
In SN74HC573-Q1 datasheet, unused input pin is recommend to tied to VCC or GND.
But if some unused channel input and output pins are floating, will it influence other used channels?
Thanks.
Johnny
Part Number: SN74HC573A-Q1
Hi,
I am supporting customer for their design w TI SN74HC573A-Q1. It is a common knowledge that all unused input terminal should be tied to VCC or GND for determined state in each channel. Is it OK to pull down all the unused…
Part Number: SN74HC573A Hi,
When OE=H, the output is Z. I connected a 30Kohm resistor in each output pin and measure the voltages on the output pins, the voltages from out 1~8 are different, pin1=4.2V, pin2=4.1V, pin3=3.2V, pin4=0.5V, .... do you know…