Part Number: SN74HCT244-Q1 Hello,
Can you please share the ESD rating (HBM) and ESD Class detail for the below listed parts,
Kindly share the request details as soon as possible.
1. SN74HCT244QPWREP 2. CD74HC153M96 3. CD74HC393M96 4. CD74HC157M96 5. CD74…
Part Number: SN74HCT244 Hi team,
I can find the absolute maximum output current +-35mA of SN74HCT244 in the datasheet, but the recommended max output current is not shown in the datasheet.
Could you please provide the recommended max output current value…
Part Number: SN74HCT244 Two questions here for VSSOP package(DGS).
1. We're confused about the operating temp in the d/s. In the device information, it says SN74xx is only specified as 85degree. but in the package information, it says 125degree for SN74HCT244DGSR…
Part Number: SN74HCT244 Hi Team
Could you please confirm whether my understanding to the input voltage tolerance range is correct? I found no specifications on datasheet but is expecting it to have the same range as Vcc.
Max: 7V
Min: -0.5V
Thanks
Part Number: SN74HCT244 Buongiorno a tutti,
Vi chiedo cortesemente la differenza tecnica e di prestazioni tecniche tra serie SN e CD per i seguenti part number?
SN 74HCT244N(PDIP) e CD 74HCT244E(PDIP) e 74HCT244(PDIP)
Part Number: SN74HCT244 Other Parts Discussed in Thread: UCC23513 , , SN54HCT244 , SN74HCT240 , TMS320F28069 , SN74LVC240A , SN74ACT244 Hi,
my customer is using this device to drive UCC23513's optocoupler input in solar inverter.
Now they need -40-105C…
Part Number: SN74HCT244 Hello,
The device has a specification of dt/dv input transition rise and fall time: max 500ns.
What happen if this spec violate?
Will it break or malfunction?
Best regards,
Katsu
Part Number: SN74HCT244
Hello team
I have question about the output current. From the datasheet , we see the current is 6mA driver at 6mA. Is the value is max or typical? if the output current is 8mA each channel, does have some risk about it? Thank…
Part Number: SN74HCT244 Hello Team
My customer is using SN74HCT244. Power supply is 5V. When the input voltage is voltage is 1.1V, the output is 2.6V. when the input is 1.4V, the output is 5V. But the VIH is 2V. So why the out have output when the input…