Part Number: SN74LV123A Hello,
We are using SN74LV123A IC in our design. we are expecting the outputs as truth table highlighted per attached image.
Our circuit is as below attached image.
Input B is as shown in the attached image below. with other inputs…
Part Number: SN74LV123A Hi,
We use the Buffer IC SN74LVC8T245RHLR in our design.
I am wrongly connected the Input voltage Range is 3.3V , but the VCC is given as 1.8V.
Shall we proceed with input voltage is more than the VCC?
Kindly confirm is there…
Part Number: SN74LV123A Hi team,
In the datasheet, K-Vcc is spec'd only for CT=1000pF, 0.01uF, 0.1uF and 1uF. But my customer wants to use CT=10uF with Vcc=3.3V or 5V. Could you show us the characteristic for CT=10uF?
Regards,
Ohashi
Part Number: SN74LV123A Other Parts Discussed in Thread: CD74HC123 Hi Team,
can you confirm that SN74LV123A can be used as an alternative for 74HC123
https://www.mouser.de/datasheet/2/916/74HC_HCT123-1525392.pdf
Thanks
Jan
Part Number: SN74LV123A
Hi,
I am working on a retriggerable multivibrator circuit, with a pulse with of 20ms for the rising edge of the pulse. I used the value of k=0.9, as the input voltage value is 3.3V. Did not work, when tried simulating in pspice…
Part Number: SN74LV123A In sn74lv123A datasheet their capacitor graph is not mentioned properly.so there is a little confusion while designing it can you please help me to design.
And thee is not proper formula for SN74lv123a to select Rext and Cext. …
Part Number: SN74LV123A Other Parts Discussed in Thread: CD74HC4538 Is there a capability to determine or simulate K factor for dedicated supply Voltage and RC combination ?
Same question relating to CD74HC4538
Part Number: SN74LV123A Other Parts Discussed in Thread: SN74LVC1G123 We are using SN74LV123AD as monostable Multivibrator for generating 15 Second and 5 Second pulse.
While testing we are not getting consistent pulse output.
It varries from 15.8 Second…
Part Number: SN74LV123A Hi team,
My customer wants to use large Cext (up to 10uF) for SN74LV123A.
So, they want to know the rough boarder for the Cext which the external clamping diode will be nessesary.
How large Cext can they use without the clamping…