I have an additional question. I understand that if you input an assert signal to the CLR pin of SN74LV273A using a reset IC, etc., and release the clear after the power is turned on, the output will be low until CLK is input. Is this understanding correct…
Part Number: SN74LV273A hi,
The Q output is occasionally not kept low even after CLR is already set at low during power-up in which the CLK and CLR ramp up speed is very low (rise speed is 3.3v/2s). The detail test waveforms are attached.
there are…
Part Number: SN74LV273A Dear expert.
My customer will face the shortage because of these tight situation, but we want to use your products.
So could you inform me what is alternative of SN74LV273APWR ?
If possible, could you check it with something in stock…
The function table is wrong; it was accidentally copied from the SN74LV273A-Q1 datasheet. The SN74LV373A datasheet has the correct table.
The initial state of a latch is undefined (either high or low). To get this latch into a known state, you would have…
Part Number: SN74LV273A Hi team,
Let me confirm thermal pad connection for just in case.
It should be connected to GND, correct?
Best regards,
Shota Mago
Part Number: SN74LV273A Dear sir:
May I have some confirming item for SN74LV273A application ?
If original our circuit use 74LVC273PW ,TI SN74LV273A part could replace it ? Or Any need consider or Risk ?
https://assets.nexperia.com/documents/data-sheet…
Part Number: SN74LV273A Hi,
We can find "Δt/Δv Input transition rise or fall rate" on datasheet. Does rise rate of this parameter mean the delta from VoL to VoH?
Thanks and best regards, M.HATTORI
Part Number: SN74LV273A Other Parts Discussed in Thread: SN74LV00A Hi Team,
Is there any graph for SN74LV273A?
- VOH vs IOH
- VOL vs IOL
Regards,
Kotaro Yamashita
Part Number: SN74LV273A Hi,I have used SN74LV273 in my design,i have two questions
1.what is the inital state of Q output,in my design is high level output,even i put clear pin low for about 20ms after power on
2.in the datasheet table 2 of truth table…