Part Number: SN74LV4051A-Q1 Now customer ask for ESD MM(Machine Model) Level for SN74LV4051-Q1 at Automotive battery module. But I can’t look for MM level in datasheet(below). Can you provide to me for ESD MM(Machine Model) Level for SN74LV4051-Q1…
Part Number: SN74LV4051A-Q1 Hi
Regarding to the SN74LV4051AQ1, have you ever experienced abnormal act caused by EMC test?
Do you have any advisory of considering EMC?
(Recommended design, layout guide, anything is ok)
BestRegards
Hi Louie
Thank you for your reply.
And sorry, my question might have not been clear.
We have to consider the countermeasure to avoiding device damage under particular situation.
(This considering is required for automotive device)
Of course, we never…
Part Number: SN74LV4051A-Q1 Other Parts Discussed in Thread: TS3A5017 , CD4051B Hi all,
I want to connect 4 Single-Wire PWM Outputs from MAX6672 channels to LPC24xx microcontroller (uC). Previously I was using 4 different timer capture inputs from the uC…
Part Number: SN74LV4051A-Q1 Hi
SN74LV4051Q1 has IIK < -20mA as absolute maxmum ratings.
If it gets IIK lower than -20mA for a moment and it backs to normal (IIK > -20mA) immediately, could the device operate in the normal status?
Could you please…
Part Number: SN74LV4051A-Q1 Hi
There are maximum ratings of Input voltage (Vi) and Switch IO voltage (Vio). The max Vi is represented by 7V, but Vio is by Vcc+0.5V.
It means the internal diode to VCC is only on the switch IO pins. (It involves -50mA …
Other Parts Discussed in Thread: SN74LV4051A , SN74LV4051A-Q1 Hi
We have questions about SN74LV4051AQ1.
1. We found the difference of absolute maximum ratings description between SN74LV4051A-Q1 and SN74LV4051A, for Input clamp current, IO diode current.(min…
Hi
We have question about the following E2E post.
We found that Iiok (IO diode current) was defined as minus value only in the datasheet.
So we assume this device has input clump diode from GND to the pins only, is it right?
If so, we think input…
Hi Clemens-san, and Rami-san,
Thank you for your prompt catch up on this this topic.
Sorry, the variant in SN74LV4051A -Q1 product folder, not SN74LV4051A. I understood that, for example, we can regard CLV4051ATDWRG4Q1 as SN74LV4051ATDWRQ1 since E4 doesn't…
Other Parts Discussed in Thread: SN74LV4051A-Q1 Hi,
My requirement is that FPGA will toggle the selection bits of the analog MUX SN74LV4051A-Q1 for every 1us to switch from one channel to next channel to provide the 8 multiplexed channels to ADC in 8us…