Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74GTL2014 , TXU0104 , TXB0104 Hi Team,
We have used SN74LV4T125PWR in our design in 3 locations and unfortunately Inputs are connected to Outputs pins & Outputs to input pins in one of the Buffer…
Part Number: SN74LV4T125-Q1 Hi Staff
SN74LV4T125-Q1
I am planning to mold SN74LV4T125-Q1, but is it possible to use it?
About molding agent Main agent: Pernox XN-2248 (clear) Hardening agent: Percure XY-2233-3 Epoxy filler, hardness 15
regards cafain
Part Number: SN74LV4T125 I have connected MISO (SDO_1 in the diagram) of slave device (SPI) to the 4A of SN74LV4T125, but at 4Y I get no data, also that the enable pin is grounded.
I am attaching the circuit diagram.
Please guide.
Regards,
Shakil
Part Number: SN74LV4T125 Dear Technical Support Team,
①Is the output current rating(Max) below due to the heat problem or the output voltage(VOH/VOL) cannot be maintained ?
② Are these specs for total channel output current or per channel?
■SN74LV4T1…
Part Number: SN74LV4T125-Q1 Other Parts Discussed in Thread: SN74LXC8T245-Q1 , TXU0204-Q1 Hi Team,
My customer is using the 74AVCH4T245PW-Q10J (TSSOP), however, it is max 3.6Vin, and are looking for 5.5Vin to translate from 5V to 1.8V.
I know we have a…
Part Number: SN74LV4T125 I have a couple of the output pins connected to gpios.
These gpios have pull up resistors to 3v3 turned on by default.
The vcc is connected to 3v3.
I tested the voltage on the input pin, which has nothing connected to them and…
Part Number: SN74LV4T125 After looking at the datasheet for the SN74LV4T125,
I do not see too much on the explanation of the OE pin.
Are the options to connect to GND or VCC?
What are the differences?
What scenarios would call for connecting to one…