Hello,
In addition to the recommendation above, there is a newly released device that is optimized for SPI buffering or level shifting:
https://www.ti.com/product/TXU0304 (commercial)
https://www.ti.com/product/TXU0304-Q1 (automotive)
It can support 1…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74LV1T125 Hello
On both the SN74LV4T125 and the SN74LV1T125, we see the Ii for the A side has current characteristics of 1uA;
do you have the maximum input current characteristics for the 3-state…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74AVC2T244
Dear Technical Support Team,
The datasheet of SN74LV4T125 doesn't have output to output skew.
Do you have any data?
Level shift from 1.8V to 2.5V.
SN74AVC2T244 has this.
Output…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74AHCT125 Hi Team,
Due to the shortage on SN74LV4T125RGYR, can we replace it with SN74LV125ARGYRG4? Thank you.
Best regards,
Mike
Part Number: SN74LV4T125 Hello TI,
We would like to know the consumption data of this part. SN74LV4T125PWR
Our application: level shifter for some control pins and 32k clock, input 1.8V & output 3.3V (VDD=3.3V)
All four channels are occupied. Thank…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74LVC3G17 , ULN2003A , TPL7407LA , CD4504B , CD40109B , UCC27517 Hello TI,
I have an applications where 3.3V to 5V and 5V to 3.3V is required
I selected SN74LV4T125 for both the cases.
Kindly let me…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74LVC125A , SN74LV1T125 Hi Team,
On one of our board, a SN74LV4T125 is used to buffer SPI clock, MOSI and CS. What is the max. frequency it supports? The SPI runs at 63MHz and I found it enlarges…
Part Number: SN74LV4T125 Hi expert,
Our customer is using SN74LV4T125 as a SPI repeater.
Customer is operating the device up/down translation at 3.3V and Vcc = 3.3V, the max frequency 20MHz
May I know the question as below?
1. The length from pch to SN…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: CD40109B , SN74AHCT125 Hi Team,
For customer requirement : 3.3V->5V for UART.(4bit) I suggest our SN74LV4T125. And I have questions showing as below.
1. Whether our level shift has protection…