Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74CBT3125 Hi Team,
Can this device be judged normally when the power supply is 4V and the input voltage is 1.8V? Look at the following indicators. When the power supply is 4.5V, it needs Min 2V…
Part Number: SN74LV4T125 Hi Team,
I received an inquiry from one customer that they faced issues with their MP product where the SN74LV4T125 fails due to the connected motor has a rise and fall time that is too slow for the SN74LV4T125. They are looking…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74AHCT125 , SN74AHC125 Hi Team, We have a customer that has the intended design with SN74LV4T125 in the image below. The customer would like to confirm the following if this would work:
1. Enable…
Part Number: SN74LV4T125 Hi Team, I hope you can help us fill in this information for our customer.
Theta Jb, Theta Jc (Top), Theta Jc (Bottom), Theta Ja, Reliability Tj Max, "Operating Tj Max", "Absolute Tj Max"
Thank you very …
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74AUP3G34 , SN74AXC4T774 Hello,
I am trying to find a part which can shift a 3.3v SPI signal to 2.8v, for an embedded TFT display application. I am struggling to understand whether any of the…
Part Number: SN74LV4T125 Hi,
What are the dimensions for the thermal pad on SN74LV4T125 for package RGY (S-PVQFN-N14)?
The data sheet does not show any footprint dimensions but links to package information documant MPQF114G: mechanical data for RGY…
Part Number: SN74LV4T125 Hi,
my customer is using SN74LV4T125 for 1.8V to 3.3V translation. And find that in some board the 1.8V input will degrade to about 1.0V.
The output is connected to MCU's IO port through a 0ohm resistor. No matter we solder or…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: LMH6881 , , SN74LVC1G14 , SN74LVC2G14 , SN74LVC3G14
Hi team,
Need to level shift a 0V logic 0 reference to -1.25V logic 0 reference for the LMH6881 device SPI working with max 50MHz SCLK frequency…