Part Number: SN74LVC125A-Q1 Other Parts Discussed in Thread: SN74LVC125A Hi,
The OE pull up resistor is determined by SN74LVC125A OE port sink current, please share the maximum value of the sink current or the typ pull up resistor value.
When maximum sink…
Part Number: SN74LVC125A-Q1 Hello team,
Is it possible to use the buffer such as SN74LVC125A-Q1 for the SPI communication with 3m cable between master and slave?
Or, can you recommend any automotive devices for the 3m SPI transmission (2ch x 4wire SPI…
Part Number: SN74LVC125A-Q1 Other Parts Discussed in Thread: MSP430F5438A Dear all,
The project is composed by two stack of electronic boards the share an SPI Port. The 2 stacks are connected by a 40cm long cable. Below you can find an image to clarify…
Part Number: SN74LVC125A-Q1 Hi team,
Can you confirm if the unsed input pin of pull down and ouput pin of floating are okay in SN74LVC125A-Q1? Can you review the following schematic?
Thanks,
Best Regards,
Sam Lee
Part Number: SN74LVC125A Other Parts Discussed in Thread: SN74HCS125 Hello Q1: My customer uses SN74LVC125A. Datasheet says input transition rise or fall rate is less than 8ns/V as follows. Is this spec applies to not only 1A to 4A but also 1OE_ to 4OE_…
At 1.8 V, the 2N7001T-Q1 indeed has more drive strength (8 mA) than LVC (4 mA).
Alternatively, use multiple LVC outputs in parallel (SN74LVC2G125-Q1, SN74LVC125A-Q1).
Part Number: SN74ABT541B-Q1 Other Parts Discussed in Thread: SN74LVC2G17-Q1 , SN74LVC125A-Q1 , SN74LVC1G17-Q1 , CD74AC541 , SN74ACT244-Q1 , SN74HCS541-Q1 We require current driving capacity of 20mA for optical transmitters. These transmitter are opetated at…
Part Number: SN74LVC125A-Q1 Hi team,
My customer is considering using SN74LVC125A-Q1. He want to calculate the dynamic power dissipation by using Cpd. However,only the typ value of Cpd is described in the datasheet. Could you please tell me the max value…
Part Number: SN74LVC126A-Q1 Other Parts Discussed in Thread: SN74LVC125A-Q1 Hi team,
Here is request from my customer shown below. I want to recommend the SN74LVC126A-Q1.
Could you please confirm following questions:
1.Do you have better recommend…
Part Number: SN74LVC125A-Q1
Hello,
Is it possible to pull up VI to 8V at 1.2 kΩ when Vcc is off? According to the datasheet input and output negative voltage ratings may exceed if the input / output current ratings are observed.
Is it okay to exceed…