Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74LVCR16245A , SN74AVCB164245 We're looking for an alternative to SN74LVC16T245, that integrates either the ~25ohm damping Res or DOC (Dynamic Output Control) circuitry. Also needs to be 5V…
Part Number: SN74LVC16T245 Hi Team,
I need to translate from 3.3V to 5.0V. I have found some schematics using pull up/down resistors on inputs/outputs. I've found some others schematics using a low resitors(like 22R) in series with inputs/outputs.…
Part Number: SN74LVC16T245-EP Hi All,
In my Project I am using one 16 bit level translator SN74LVC16T245MPWREP, one 8 bit level translator SN74LVC8T245MPWREP, one 2 bit level translator SN74LVC2T45MDCTTEP in which signals are connected to a Micro D connector…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74LVC1T45 , SN74LVC2T45 , SN74LVC8T245 , Dear Team,
The customer is looking for a lower channel count with 16bits device.
Do we have a suitable device?
It seems we don't have lower than 8 channel…
Part Number: SN74LVC16T245 Hi team. My customer wants to put in capacitance at the output for noise. How much capacity can I insert? The datasheet says it is 10pF(MAX). Is my understanding correct? If it is correct, how about capacity when other VCC. Sincerely…
Part Number: SN74LVC16T245 Hi,
Can I tie together all 1Bx to 2Bx? The goal is to use 1Ax as inputs (1Bx outputs) and 2Ax as outputs (2Bx inputs)? I mean can I have impedance problems tying together 1Bx and 2Bx? To achieve this 1OE, 2OE, 1DIR and 2DIR…
Part Number: SN74LVC16T245 Hi team,
The board including the following circuits works normally but sometimes Problems may occur on. Please tell me how to use the device.
■Current usage As shown in the figure below, the output signal from BCT245 (TTL) is…
Part Number: SN74LVC16T245 Hi team
SN74LVC16T245
I want to ask if I have to connect /1OE, /2OE, 1DIR, 2DIR pin to VCCA through pullup resistor separately?
Is it possible to connect /1OE, /2OE to VCCa with a pull-up resistor?not two.
Is it possible to connect…
Part Number: SN74LVC16T245-EP Dear Sir,
We are planning to use SN74LVC16T245-EP in our existing design.
In view of the above we want to know the end of life of the product.
Regards, Arun P