Part Number: SN74LVC1G125-Q1 Other Parts Discussed in Thread: PCA9306 Hello TI engineer,
In our design ,we use SN74LVC1G125-Q1 as buffer for SMI bus,i want to know if i can use PCA9306DCUR(an level -shift device) to replace SN74LVC1G125-Q1. Are there…
Part Number: SN74LVC1G125
Hi, Support Team
SN74LVC1G125DSFR (SON6) is 1mm x 1mm, but datasheet show SON(6) 1.45mm x 1mm is correct?
if any, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: SN74LVC1G125
Hi, Support Team
as we know DSF is called SON or X2SON, have any note in datasheet?
if possible, please provide us SN74LVC1G125DSFR the right datasheet.
Package materials information show DSF is (SON)
Package outline show DSF…
Part Number: SN74LVC1G126 Other Parts Discussed in Thread: SN74LVC1G125 , , SN74AHC1G125 , SN74AUP1G125 Both parts SN74LVC1G125 & 126 testing on the same test parameter “ Sensor Status Bits Test ” . The SN74LVC1G126 is an alternative MPN…
Part Number: SN74LVC1G125 Hi All,
I have a question about the ESD of the SN74LVC1G125.
Regarding the following ESD description, HBM is from 0 to 2kV. Are you testing -2kV (minus) HBM? Are you testing at -1kV for CDM as well?
Best Regards, Ishiwata
Part Number: SN74LVC1G125 Hi Team,
Could you please help to check what does this comment mean:
(2) The input and output negative-voltage rating may be exceeded if the input and output current ratings are observed.
I want to known if this requirement…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74LVC1G126 What's the major difference between SN74LVC1G125 and SN74LVC1G126 from process and wafer point's of view? i don't see the difference in comparison table. Very thanks. …
Part Number: SN74LVC1G125 Hi Logic Team,
Can you please provide the following specifications for the SN74LVC1G125DBVR, which I was unable to find in the datasheet?
Output voltage for Active State and Three-State
Output capacitance
Maximum power dissi…
Part Number: SN74LVC1G125
Hi,
Is there any advance in using LVC1T45 over LVC1G125 for logic level translation from 3.3V to 1.8V? I checked datasheet and parameters for both devices are identical.
I prefer to have output in high-Z without changing direction…