Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74LVC1G126 What's the major difference between SN74LVC1G125 and SN74LVC1G126 from process and wafer point's of view? i don't see the difference in comparison table. Very thanks. …
Part Number: SN74LVC1G125 Hi Logic Team,
Can you please provide the following specifications for the SN74LVC1G125DBVR, which I was unable to find in the datasheet?
Output voltage for Active State and Three-State
Output capacitance
Maximum power dissi…
Part Number: SN74LVC1G125
Hi,
Is there any advance in using LVC1T45 over LVC1G125 for logic level translation from 3.3V to 1.8V? I checked datasheet and parameters for both devices are identical.
I prefer to have output in high-Z without changing direction…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74AUC1G125 ,
Hi team,
my customer found there's no clock signal when used our buffer,
please noted that R735 is DY (the one below).
all signal level is 1.8V .
as you can see the blue and…
Part Number: SN74LVC1G125 Hi Expert
In datasheet 10.2.1, there mentioned: The high drive will also create fast edges into light loads so routing and load conditions should be considered to prevent ringing.
What does the light load mean here? Is it a kind…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74LV1T125 , SN74AHCT1G125 Hello,
We are considering using this part for our product, however the issue is that we are expecting to power this with a 5.15V source (USB), however the input is about…
Part Number: TPS62091 Other Parts Discussed in Thread: SN65HVD1781 , SN74LVC1G125 ,
Hi.
This circuit is designed to, when the 5V rail is turned on, 1.3s later the 3.3V rail is turned on. SN65HVD1781 is supplied on 5V rail, and at startup it will be set as…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: TI-API When attempting to order part SN74LVC1G125 using part number SN74LVC1G125DCKR I get the error message "Item is not fully scheduled". Having an understanding of what this means will allow…