Part Number: SN74LVC1G125-Q1 Other Parts Discussed in Thread: SN74LVC1G125 Hi team,
I have some questions about SN74LVC1G125-Q1.
As below image.
My question is
1. Why do we have two Vcc condition. I mean when condition1 Vcc = 1.65V to 5.5V and the IOH…
Part Number: SN74LVC1G125-Q1 Hi There,
I used "1P1G125QDCKRQ1" of SN74LVC1G125-Q1 Series. Some have package information.
http://www.ti.com/jp/lit/ds/symlink/sn74lvc1g125-q1.pdf
The device information on the first page is "SOT-23(5)".…
Part Number: SN74LVC1G125-Q1 Other Parts Discussed in Thread: SN74LVC1G17-Q1 According to the datasheet, the input Max rise/fall time is 5ns/V, but in my design, it is 50ns/V, this will cause problem? like no output triggered? (no speed requirement for…
Part Number: SN74LVC1G125-Q1 Hi TI support,
I intend to use partial power down feature of SN74LVC1G125-Q1 in one of my application. I would appreciate some clarifications on this feature,
1. Datasheet doesn't specifies condition of OE/ while specifying…
Part Number: SN74LVC1G125-Q1 Dear Team,
Could you please explain the parameter measurement section.And also i need to know that, how Vload can be 2 x Vcc.
Pls do the needful.
SN74LVC1G125-Q1
Part Number: SN74LVC1G125-Q1 Other Parts Discussed in Thread: SN74LVC1G125 Hi TI-team
SN74LVC1G125-Q1 has no SPICE model.
But SN74LVC1G125 has SPICE model.
Please tell me why there is no SPICE in automotive products.
Best Regards,
Koji Hayashi
Part Number: SN74LVC1G125-Q1 Other Parts Discussed in Thread: SN74LVC1G125 Hi,
We only define Tpd when Vcc is 3.3V or 5V in the datasheet. May I know what is Tpd value if Vcc is 1.8V?
Thanks!
Antony
Part Number: SN74AXC4T774-Q1 Other Parts Discussed in Thread: SN74LVC1G125
Hi,
SPI devices configured in the device as shown below. MISO line is output from Level shifter.
When SPI slave-2 driving MISO line, working as expected.
When SPI slave-2 driving…
Part Number: SN74LVC1G125-Q1 Hello
What is the recommend output current at Vcc=3.3?
The SN74LVC1G125-Q1 . SGES002C–APRIL 2003–REVISED APRIL 2008 datasheet (pg3) shows 16ma and 24ma for Vcc=3v.
The datasheet front page states "±24-mA Output Drive…