Below the minimum recommended supply voltage of 1.65 V, correct operation is not guaranteed. In particular, the output will not be able to drive low as long as the gate threshold voltage of the internal MOSFETs has not yet been reached.
Devices with …
Part Number: SN74LV1T126 Other Parts Discussed in Thread: SN74LVC1G126-Q1 , SN74AHCT1G126-Q1 , TXU0101-Q1 Team,
Would like to check if we have Q-grade spin for SN74LV1T126, or any similar alternative, to suit customer's automotive design that requires AEC…
Other Parts Discussed in Thread: SN74LVC1G126 , SN74LVC1G240 , SN74LV125A , SN74LVC1G126-Q1 Hi, Do you have a data which express the typical value, distribution and/or statistical data of Tpd? Thank you for your support in advance. Regards, Ken Other reference…
Other Parts Discussed in Thread: SN74LVC2G34-EP , SN74LVC1G126-Q1 , SN74LVC1G126
Hello,
If an output from SN74LVC2G34-EP or SN74LVC1G126-Q1 is pulled up to 3.3V through a 10kohm resistor while the device is unpowered, is that okay? Or could it damage the…
Hey Jingyuan,
If the input is floating then the voltage can drift pass the switch threshold causing the output to switch. You can use the SN74LVC1G126-Q1 which has an output enable. If you connect that OE input through a pull-up to the supply of driver…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…