Part Number: SN74LVC1G32 Hi Team,
Good day, can you help with the inquiry below?
I want to drive another circuit from the output of the OR gate SN74LVC1G32DCKR, what if I do not supply power to the TI OR gate and have an active input, will the IC still…
Part Number: SN74LVC1G32 Hi Team,
May I know how to achieve following function?
SN74LVC1G32 is applied on power disable function.
We would like to achieve debounce time of input signal function.
For example, <1us signal drop would not trigger SN74LVC1G32…
Part Number: SN74LVC1G32-EP Hello
Can you share the thermal resistance information of this device SN74LVC1G32-EP specifically the junction to case (ƟJc)?
Thanks
Part Number: SN74LVC1G32 Hi Expert,
I find a strange things in SN74LVC1G32 and SN74LVC1G32-Q1 datasheet. I suppose these two are only different for auto version. As for package, they should be in the same size. But I find they have different size even…
Part Number: SN74LVC1G32 Other Parts Discussed in Thread: SN74LVC1G97 Hi Sir,
With SSD application, SN74LVC1G32 is applied on power disable function. we'd like to debounce time of input signal.For example, <1us signal drop would not trigger SN74LVC1G32…
Part Number: SN74LVC1G32 Other Parts Discussed in Thread: SN74LVC1G07 Hi TI Team,
I have one doubt regarding SN74LVC1G32QDCKRQ1 OR Gate IC.
If i am connecting this IC VCC Pin 5V and and IC out put side pin we connected 1K resistor through 6.5V for other…
Part Number: SN74LVC1G32 Hi Team,
Please help to check does SN74LVC1G32DSF2 fully same with SN74LVC1G32DSFR?
Only different on Pin1 Quadrant ?
Thanks!
Kai
Part Number: SN74LVC1G32 What is the difference between SN74LVC1G32DSF R and SN74LVC1G32DSF 2 ? I show the lead finish is different between the 2 but both are 5K reels. Does this means there are 2 different build locations? Is there a performance difference…