Part Number: SN74LVC1T45-Q1 Hi, Support Team
do we have SN74LVC1T45-Q1 of functional safety document?
(Functional Safety, FIT Rate, Failure Mode Distribution and Pin FMA)
if any, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: SN74LVC1T45-Q1
Hi, We added a Zener circuit for on VCCA for overvoltage protect as below. Could you please help to check if the capacitance of C4324 enough for this change? Moreover, is there any expectable issue about back feed for this change…
Part Number: SN74LVC1T45-Q1 Other Parts Discussed in Thread: SN74LVC1T45 , SN74LVC1G126-Q1 Dear team,
My customer is using SN74LVC1T45-Q1 as level-shifter for SPI signal between high-side driver and MCU in body control module as illustrated below:
The…
Part Number: SN74LVC1T45-Q1 Other Parts Discussed in Thread: SN74AXC4T774 , SN74LVC1T45 Hi,
As shown in the datasheet of SN74LVC1T45-Q1.
"In a bidirectional application, these enable times provide the maximum delay from the time the DIR bit is switched…
Part Number: SN74LVC1T45-Q1 could you tell me what the Aport/Bport states are in below condition?
1. Either VCCA or VCCB is below 1.65V and other side is above 1.65V
2. VCCA=VCCB=GND, DIR=X(dont care)
3. VCCA=GND, VCCB=1.65V~5.5V, DIR=X(dont care)
Part Number: SN74LVC1T45-Q1 Hi Team,
I can see around 150uA leak current with following condition. Does this opperation have any issue?
VCCA: 5V
VCCB: <300mV
DIR = GND = 0V
Regards,
Kotaro Yamashita
Part Number: SN74LVC1T45-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 , SN74AXC1T45-Q1 , TXS0102-Q1
Dear Support Team,
We are looking for alternate part for SN74LVC1T45-Q1 with Dual bit and Dual direction selection part.
For UART design, Checking…
Part Number: SN74LVC1T45 Hi Experts,
I have two questions about SN74LVC1T45 power-up sequence.
Q1. The SN74LVC1T45 PCN adds the following new power-up sequence recommendations: Does the SN74LVC1T45 manufactured before PCN require the same power sequence…
Part Number: SN74LVC1T45-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 I see the following in the SN74LVC1T45-Q1 datasheet:
A proper power-up sequence is advisable as listed in the following:
1. Connect ground before any supply voltage is applied…