Part Number: SN74LVC2G04 Hello,
we have to assemble on a pcb your part nr SN74LVC2G04DRLR (packaging SC70). On the component there are two references: a long dash and a dots. We would like to understand what is the pin nr 1 in order to get the right orientation…
Part Number: SN74LVC2G04 Dear all:
I'm FAE from WT. I have a customer use SN74LVC2G04DCKR to make a switchboard. However, after mass production of 1000 pieces, 10 pieces of the inverter input high level and cannot get low level. The following is the…
Part Number: SN74LVC2G04 Customer requesting the below information:
maximum thermal design power,
maximum junction temperature (Tjmax) operating and absolute,
junction-to-case thermal resistance (Theta JC),
junction-to-board thermal resistance (Theta…
Part Number: SN74LVC2G04 Hello Team,
My customer used SN74LVC2G04, and they only use one channel 1A/1Y, below are their schematic, pcb and test waveforms.
When 1A has a level transition, we can find there is big noise of VCC. If they set the scope to…
Part Number: SN74LVC2G04 Hello Team,
For 3.3V application, the max Voh is 0.5V@24mA, but the ASIC Vil is 0.3V, so there should be risk.
Can you share the internal circuit of this part? Why the Voh is different when there is different Ioh? Thanks
Regards…
Part Number: SN74LVC2G04 Hi,
I am looking for the thermal metrics for the following PN: SN74LVC2G04DCK.
I am looking for :
Thermal Resistance from junction to board (theta-jb)
Thermal Resistance from junction to case (theta-jc)
Thermal Resistance from junction…
Part Number: SN74LVC2G04 What's the behavior for the output rail of the inverting logic when power VCC is shutdown (it means the VCC is dropping down to below UVLO threshold point)?
In the motor gate driver application, when there are some unexpected…