Part Number: SN74LVC2G157 I'd like to simulate circuit with SN74LVC2G157DCUT, used in an new design and need PSpice model or other kind of model with which I can simulate it by Tina or LTspice.
Can you share such model to me?
Thanks
Part Number: SN74LVC2G157 I want to use the SN74LVC2G157 to select between two clocks and I want to know what the max clock rate is for an input to the device. The datasheet specs the tpd, but I can't find any clock on the minimum tw, as shown in figure…
Part Number: SN74LVC2G157 Other Parts Discussed in Thread: SN74AHC157 , , SN74HCS157 , TMUX1574 , SN74LV4053A Hi team,
My customer is looking for an 2:1 I2S MUX and I found SN74LVC2G157 and SN74LV4053A .
Are these devices good enough for customer's request as…
Part Number: SN74LVC2G157
Hi Team,
The datasheet of SN74LVC2G157 shows the Tpd between A, B, A bar, G bar and Y or Y bar. Or customer would like to know the time delay between Y and Y bar. Do we have this information?
Regards,
Danilo
Part Number: SN74LVC2G157 Hi. We want to get the SN74LVC2G157DCU with NiPdAu plating only. Is specifying the 74LVC2G157DCURG4 guarantee that we will only get NiPdAu and not tin?
Thank you.
Other Parts Discussed in Thread: SN74LVC2G157 Hello, I'm Hidetoshi Matsunami.
I would like to ask the SN74LVC2G157 Icc.
Does SN74LVC2G157 have the configuration that this device flows excess current(Icc) when the voltage of pin 6 and 7 are lower than…
Other Parts Discussed in Thread: SN74LVC2G157 Hello,
are there any data available regarding the propagation delay variations between these chips. In an existing design there are three of them inserted in different lines of a communication interface an…
Hi Esra,
routing a clock signal via a pin header is not ideal. That will harm the signal integrity. A better way of doing that is to use a multiplexer. For example LMK00105 for high performance or this SN74LVC2G157. Here you can use a pin header to select…
Hello Brian, It is I2S. sn74lvc2g157 and sn74cbtlv3257 are good device? I found below thread. Max frequency is 24MHz. https://e2e.ti.com/support/logic/f/151/t/799212 Best Regards, Fujiwara