Part Number: SN74LVC2G241 Hi,
We have a new application that uses your SN74LVC2G241DCTR dual buffer. In our case we are only using the second buffer. Pins 1 (1OE) and 2 (1A) are tied to GND. Pin 8 (VCC) is tied to a 3.3V supply via an LT1761-3.3 regulator…
Part Number: SN74LVC2G241 I am using SN74LVC2G241 in my design and i want to confirm one point regarding the same.
when the input signal at 1A pin is undefined, output will also be undefined and it ll cause damage to the target device, so is it ok if…
Part Number: SN74LVC2G241 Hi,
I have been notified of a discrepancy between the max operating temperature under the recommended operating conditions section and the ordering section.
The first states 85C, the second 125C.
Which of the two is correct…
Part Number: SN74LVC2G241 Other Parts Discussed in Thread: SN74LVC2G125 Hello,
I need a 2-bit tri-state buffer for 3.3V logic with a small delay (~ 4 ns). I also want a small package. It's a commercial, low cost application.
I thought the SN74LVC2G241…
Part Number: AM3358 Other Parts Discussed in Thread: SN74LVC2G241 UART0 is receiving characters when there is nothing connected to it. Some sequences of characters are very similar to characters that were recently sent out the UART0 port, some are seeming…
Hi Hari,
I believe Noel replied to this query already.
Figure 5 in the datasheet ( http://www.ti.com/lit/ds/symlink/sn74lvc2g241.pdf ) implies operation >60 MHz which should work for your customer's requirement (15MHz Max)
Regards
Arvind Srid…
To prevent voltage applied to the I/O of the AM335x you can use a level translator or a buffer IC. To achieve this on the BeagleBone for example the SN74LVC2G241 is used for the UART console header. This prevents UART activity from harming the AM335x…
Oh, sorry, when you said "Debug port" I was thinking the JTAG. I see the UART is labeled "Debug Port". Now I'm with you... This UART port looks problematic to me. I think you're going to end up damaging a lot of boards this way. In fact, you may have…
Hi Brad,
we have several UARTs in use in the product, there are two external ports which use a SN74LVC2G241 to interface to the FTDI usb-to seral cables we have. There is one internal GPS connection to a UBLOX device which is also 3.3V device.
I…