Part Number: SN74LVC2G74-Q1 Other Parts Discussed in Thread: SN74HCS74-Q1 Tool/software: Hi team,
Do you know if we have output Q level flip issue when 500V HBM ESD test in PRE/CLK/Q pin? my customer found this issue and want to know why.
BR
Amber
Part Number: SN74LVC2G74-Q1 Tool/software: Hi, experts.
I expect the Q output to be low When the device is powered on, So I use RC delay circuit to make CLEAR pin low firstly ,.Can this design ensure that the power-on output is low? and how much delay should…
Part Number: SN74LVC2G74-Q1 Tool/software: Hi,
Need Spice models of SN74LVC2G74QDCURQ1 device .Unfortunately it's not available on TI website.
Regards
DIlip
Part Number: SN74LVC2G74-Q1 Tool/software: Hi team,
We have some questions about the working current of several materials that we would like to confirm with you:
(1) When the working voltage of the latch SN74LV373 is 5V, is the maximum working current…
Hi,
I am trying to use this D Flip-Flop in an application where a set of push button controls the output state of the chip. I don't need a clock signal, just that the output state be held until the next event state.
The datasheet doesn't make it…
Part Number: SN74LVC2G74-Q1 Hi Team,
My customer wants to know the CDM ESD classification level of SN74LVC2G74-Q1.
Could you help provide it?
Thanks,
Molly
Part Number: SN74LVC2G74-Q1 Hi team,
Our customer is using SN74LVC2G74-Q1 in their design.
There is a capacitive load connectted the output pin and will result a 120mA/70ns pulse to the output pin.
I have not found the parameters related to this in…
Part Number: SN74LVC2G74-Q1 Other Parts Discussed in Thread: SN74HCS74-Q1 Posting on behalf of Balazs Kelenvolgyi:
A customer asked me why the input transition rise or fall rate is defined so short (5nS) in the datasheet of SN74LVC2G74QDCURQ1? They want…