Part Number: SN74LVC2G74-Q1
Dear team,
My customer wants to know below questions, could you please help answer? Because they need to compute thesystem's total Ioff which exceeds the requirements now. Their VCC is 5V.
what is the max Ioff when the…
Hi Charlie,
Charlie Xiao said: What is the difference between SN74LVC2G74 and SN74LVC1G74?
They are electrically identical devices.
The SN74LVC1G74 is available in these packages: DCT, DCU, DQE, RSE.
The SN74LVC2G74 is available in packages: DCT, DCU,…
Part Number: SN74LVC1G175 Other Parts Discussed in Thread: SN74LVC2G74-Q1 , SN74LVC1G79-Q1 Hi Logic team,
Can you suggest us any p2p automotive grade part to SN74LVC1G175DBVR (SOT-23 (DBV) | 6)?
Best regards,
Eric.
Hi Kygo,
The SN74LVC2G74-Q1 is an 8 pin positive edge triggered D flip flop with Clear and preset offered in the DCU package.
The recommended operating conditions of these devices are the same and the electrical characteristics are very similar.
Below are…
The SN74LVC2G74-Q1 has one channel, despite the name.
Two-channel devices (SN74HCS72-Q1, SN74LVC74A-Q1, SN74HCS74-Q1, SN74AHC74Q-Q1, SN74LV74A-Q1) are cheaper.
Part Number: SN74HCS72-Q1 Other Parts Discussed in Thread: SN74LVC2G74 Dear team,
Recently my customer wants to use our SN74HCS72-Q1 to replace NLV1403BDR2G, and they have two questions about our device.
1. Before they use NLV1403BDR2G, when this device…
The datasheet is correct (also see [FAQ] What is the default output of a latched device? (Flip-Flop, latch, register) ). This flip-flop requires a clock cycle to go into a defined state.
The SN74LVC2G74-Q1 has preset/clear inputs.
Hi Fery, I am assuming you need only a single flip-flop, with a preset and clear. Are there other specifications or will the SN74LVC2G74-Q1 work? Thanks! -Karan
Part Number: SN74LVC2G74 Other Parts Discussed in Thread: SN74LVC1G17 , SN74HCS74-Q1 , SN74AUP1G97 , SN74LVC1G97 , SN74HCS08-Q1 Hi Sirs,
Sorry to bother you.
We have use 2G74, schematic as below
We meet the output Q had wrong active. We tried remove D3, R4…