Part Number: SN74LVC2GU04 Tool/software: Dear Support,
we have been using this part in dck package
i am reaching out to see how can we get some bare die of this part?
thanks
Sean
Part Number: SN74LVC2GU04 Other Parts Discussed in Thread: SN74LVC2G14 , SN74LVC1GX04 , SN74LVC2G34 Hi team,
Could you please help me to pick up right inverter for crystal oscillator?
The input voltage is 3.3V. The oscillation frequency is 20-40MHz.
The…
Part Number: SN74LVC2GU04-Q1 Hi Team,
How much is the supply power's current about the max. and typ. value?
The output currents are given only, but the supply current is not.
Regards,
Haury
Other Parts Discussed in Thread: SN74LVC2GU04 , TLV3201 , TLV7011 , TLV7012 Hi,
We are looking at TAS5001-5122C2EVM Application Report. Attached here.
0451.DASF00654 (1).pdf
Have one question on SPDIF input to SN74LVC2GU04.
SPDIF input after C100 is pure…
Part Number: SN74LVC2GU04 In the Absolute maximum ratings the Output clamping current is given for the condition "Vo<0".(SCES197N )
This would indicate that there is no clamping diode to Vcc.
The same applies to 74LVC1G14 or 74LVC1G125 etc…
Part Number: SN74LVC2GU04 I have cases where a capacitive load might be driven from the other side. In that case a current is driven into the output and possibly the clamping diodes. The datasheet specifies 50mA as the absolute maximum rating. Is this…
Part Number: SN74LVC2GU04 Other Parts Discussed in Thread: TINA-TI My name is uesaka of ICOM Corporation. The HSPICE of SN74LVC2GU04 posted on TI's website is encrypted and cannot be used.
Can I send the HSPICE of SN74LVC2GU04 that is not encrypted…
Part Number: SN74LVC2GU04 Hi,
I am looking for the logic input pin impedance. The capacitance is given on the spec sheet but there is no resistance.
Is there a resistance to ground? 1Mohm?
Thank you!
-Alberto