Part Number: LMG2100R044 Other Parts Discussed in Thread: SN74LVC3G14 , , LM5156 Hi
The circuit diagram is designed with the following specifications.
-SPEC-
Input: dc24V
Output: dc 80V 5A
Part: LM5156,LMG2100R044,SN74LVC3G14
I'd like to get a review, but…
Hi Clemens,
Thank you for your information.
- SN74LVC1G14 1ch 1.65V-5.5V
- SN74LVC3G14 3ch 1.65V-5.5V
- SN74LVC1G14 6ch 2V-3.6V
Could you please explain why the voltage range of the SN74LVC inverter is different for each channel as shown above? Will a 6…
Part Number: SN74LVC3G14 In the past,We use the "SN74LVC3G14DCU3".
But now we can't order the "SN74LVC3G14DCU3"
PLEASE TELL ME THE DIFFERENCE BETWEEN"SN74LVC3G14DCU3" AND "SN74LVC3G14DCUR".
Can I use the "SN74LVC3G14DCUR…
Part Number: SN74LVC3G14 Hi, Could you tell me about SN74LVC3G14DCUR power dissipation spec? Customers are considering replacing Renesas with TI. However, TI's logic products do not have power dissipation listed. Could you tell me power dissipation specifications…
Part Number: SN74LVC3G14 Dear Specialists,
My customer'd like to adopt SN74LVC3G14 and has a question. I would be grateful if you could advise.
---
What is the latch-up immunity current?
Generally, it is specified JESD78 as 100mA.
is this device the…
Hi,
I received the following question from my customer.
Could you make sense it?
It is mentioned "Inputs Accept Voltages to 5.5V" on the datasheet.
What does it mean?
(Is this related with VI of Absolute Maximum Ratings? I'm confusing because…
There are no devices with bus-hold inputs and less than eight channels. The SN74LVTH540 would be simple, but large.
You can build a bus-hold circuit with a three-channel inverter (SN74LVC3G14), or an inverter and a buffer (SN74LVC1G14, SN74LVC1G17).
Hi Chase,
Thank you for the continued information and updates.
There could be more ringing seen at the FET gates. This can be checked by probe to see if it is a concerning amount.
For questions on the SN74LVC3G14, please start a new thread with this…