Part Number: SN74LVC3G17
I tried to simulate schmitt trigger using Ltspice and the given photo is the output with the circuit. The output does-not align with the values given in the data sheet. May i know on what changes to make to get output as per…
Part Number: SN74LVC3G17 Other Parts Discussed in Thread: SN74HC14 I am planning to use a schmitt trigger to reduce the noise from camera signal. I am not sure on what parameters to consider and choose.It will be of great help if the difference between…
Part Number: SN74LVC3G17 Other Parts Discussed in Thread: SN74AHCT125 , SN74LXC2T45 , SN74LXC1T45 , SN74LV1T34 Is SN74LVC3G17 able to do the below two scenario for level shifter application in MD sector?
VCC=5V, Input High Level=3.3V (I think this should…
The SN74LV1T34 datasheet specifies a worst-case ΔI CC of 1.5 mA for a 3.4 V input signal. However, the typical ΔI CC will be zero (see the AHCT curve):
Part Number: SN74LVC3G17 We are using SN74LVC3G17 as driver for optical transmitter. The current is almost 24mA each channel.
During Switcting we observe a ringing upto 1V.
Could there be any method to improve the signal integrity at high frequency.
…
Part Number: SN74LVC3G17
Hi Team
We are using an SN74LVC3G17 as a buffer for 24Mhz Signal. The input of the buffer is about 3.3V peak to peak. In the output, we have kept a variable pot of about 0 - 500 Ohm.
While we change the pot, We are also getting…
Part Number: SN74LVC3G17 Dear Team,
SN74LVC3G17 has the inputs overvoltage tolerant feature, and the datasheet describes as follows, - Inputs are overvoltage tolerant allowing them to go as high as 5.5 V at any valid VCC.
What does the "at any valid VCC…
Part Number: SN74LVC3G17 Hi Team,
May I know how to distinguish marking code with SN74LVC3G17DCUR ?
I don't understand our mention in the table, which one should I follow? Is that CZ ?
What is "(17, C17J, C17Q, C 17R)" mean ?
Thanks for…
Part Number: SN74LVC3G17 Hello,
I use the SN74LVC3G17 as a buffer, the input pins are connected to buttons and pull up to Vcc, output pins are connected to micro controller, Vcc is +1.8V.
It is because I use CR2032 coin battery as power source, I would…
Part Number: SN74LVC3G17 Other Parts Discussed in Thread: TLV9034 My application has a weak power supply (simple resistor-zener diode) and I noticed that the supply voltage drops when the input voltage off one of the inputs of the 74LVC3G17 is not 0V or…