Part Number: SN74LVC8T245-EP Other Parts Discussed in Thread: SN74LVC8T245 Hello,
How can I determine if a part is manufactured using copper bond wires or other metals such as gold? The reason I ask is because the government requires additional acceptance…
Part Number: SN74LVC8T245-EP Other Parts Discussed in Thread: SN74LVC244A , SN74AUP1G17 , SN74AUC1G17 , SN74AXC1T45 Dear all:
Unfortunately, I don't have so much experience with logic yet. That's why a have a fundamental question regarding Buffers and…
Part Number: SN74LVC8T245-EP Other Parts Discussed in Thread: SN74LVCC4245A-EP SN74LVC8T245-EP accepts 5V CMOS inputs with VCC = 5V, Is there a translator the same like SN74LVC8T245-EP but accept TLL inputs with VCC = 5V? I know we can change VCC to 3…
Part Number: SN74LVC8T245-EP Other Parts Discussed in Thread: CD74HCT423 , SN74HC244 , SN74LVC8T245 Hi,
For level shifting certain logic from LVTTL (3.3V) to TTL (5V) logic I have incorporated SN74LVC8T245MDWREP and CALVC164245MDGGREP for Octal and 16 bit…
Part Number: SN74LVC8T245-EP In TI data sheet, There are two part numbers with VQFN package.
What is the difference between V62/09615-01ZE and CLVC8T245MRHLTEP? It seems that two parts have the same electrical and environmental and mechanical characteristics…
Part Number: SN74LVC8T245-EP Hi,
i am looking for the power dissipation of the device SN74LVC8T245-EP, when VccA = 3.3V and VccB = 5V. Similarly for the SN54LVT162245A device.
Thanks
Ishank Varshney
Part Number: SN74LVC8T245-EP I have an application for this part where I am taking in TTL logic and transititioning it to FPGA logic levels. TTL is 5V logic and is defined as having the following parameters:
High Output = 2.7V - 5V
Low Output = 0V - 0…
Part Number: SN74LVC8T245-EP Hi,
We have selected and procured the following component for our project.
SN74LVC8T245MPWREP
The end customer wants details regarding operating temperature and grade (like Automotive, Military) which we couldn't find in…
Hi Anand,
There is a new 5V translator that we are working on to release for space applications. Presently the roadmap looks like the device samples will become available around March with full release in October. There is one existing SN74LVC8T245-EP…