Part Number: SN74LVC8T245-Q1 (a) When both Vcca and Vccb is 0V, before turn on SN74LVC8T245PW, are there the recommended voltage and current of A1 and B1? Are the voltage limits at turn-off the same as the range in the datasheet (Absolute Maximum Voltage…
Part Number: SN74LVC8T245-Q1 TEam,
Working a power budget for a project,
From the datasheet, the max current in 8.1 is the “Continuous output current ±50 mA Continuous current through each VCCA, VCCB, and GND” at +/- 100mA.
So 100mA…
Part Number: SN74LVC8T245-Q1 Other Parts Discussed in Thread: SN74LVC8T245 Hi,
Could you please share the SN74LVC8T245 the pin/out package of the DW package (SN74LVC8T245DWR) in SOIC-24.
I think on the datasheet I can only find the DB, DBQ, DGV, PW or…
Part Number: SN74LVC8T245-Q1 Hello,
I plan to use SN74LVC8T245-Q1, but I already have data on SN74LVC8T245PWG4.
Do they share the same die ?
I think the question has already been asked, but the thread appears deleted...
Best regards,
Dr. Vincent Bo…
Part Number: SN74LVC8T245-Q1 Team,
My customer is trying to evaluate worst case current consumption so that they can size our power rails accordingly:
How do I evaluate maximum current draw on the translators inputs (on side VCCA for example)?
Is there…
Part Number: SN74LVC8T245-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 Hi Team,
I am using SN74LVC8T245-Q1 8-bit dual supply bus transceiver to interface serial flash (3.3V logic) to controller at 5V supply.
The device SN74LVC8T245-Q1 has direction…
Part Number: SN74LVC8T245-Q1 Hello e2e,
SN74LVC8T245Q Quality and Reliability folder states to look in the datasheet for ESD, HBM CDM, details. The details are not in the datasheet.
Please provide. Thank you
Part Number: SN74LVC8T245-Q1 Other Parts Discussed in Thread: SN74AXC8T245-Q1 I see the following note in the SN74LVC8T245-Q1datasheet:
"To ensure the high-impedance state during power up or power down, nOE should be tied to VCC through a pullup resistor…
Part Number: SN74LVC8T245-Q1 Hi Team,
My customer now is evaluating our SN74LVC8T245-q1 in new project. Schematic as below:
Configuration is B data to A. But when customer test, it was found that B1-B3 are low voltage, while A1-A3 are high voltage. A1…
Part Number: SN74LVC8T245-Q1 This is Joong-hyeok Lee, DMSMS researcher of Leoinnovision. Leoinnovision is the official EOL(End Of-Life)/obsolescence part manager of Korean Military (Army, Navy, Air force) and PLM agency of many defense industries (Hanwha…